This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Resolution of JPEG Decoder in RDK 01.09.00.16 not supported yet?



Hi,

We found the jpeg decoder in RDK 01.09.00.16 could not return the correct frame resolution, which its version is 01.00.02.00.

The h264 and h263 decoder can return the frame resolution correctly, which rely on one variable "displayBufs".

Is this feature going to be supported in the next release? Thanks.

Yuanchi Yu