Other Parts Discussed in Thread: OMAP3530
Hi all,
I am trying to create a bootable SD card for my OMAP3530 EVM. For that I am following the following steps:
honey@honey-desktop:~$ sudo fdisk /dev/sdc
WARNING: DOS-compatible mode is deprecated. It's strongly recommended to
switch off the mode (command 'c') and change display units to
sectors (command 'u').
Command (m for help): d
Partition number (1-4): 1
Command (m for help): d
Selected partition 2
Command (m for help): p
Disk /dev/sdc: 3963 MB, 3963617280 bytes
255 heads, 63 sectors/track, 481 cylinders
Units = cylinders of 16065 * 512 = 8225280 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes
Disk identifier: 0x46e28938
Device Boot Start End Blocks Id System
Command (m for help):
Command (m for help):
Command (m for help): n
Command action
e extended
p primary partition (1-4)
p
Partition number (1-4): 1
First cylinder (1-481, default 1):
Using default value 1
Last cylinder, +cylinders or +size{K,M,G} (1-481, default 481): +121
Command (m for help): p
Disk /dev/sdc: 3963 MB, 3963617280 bytes
255 heads, 63 sectors/track, 481 cylinders
Units = cylinders of 16065 * 512 = 8225280 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes
Disk identifier: 0x46e28938
Device Boot Start End Blocks Id System
/dev/sdc1 1 122 979933+ 83 Linux
Command (m for help): t
Selected partition 1
Hex code (type L to list codes): 6
Changed system type of partition 1 to 6 (FAT16)
Command (m for help): p
Disk /dev/sdc: 3963 MB, 3963617280 bytes
255 heads, 63 sectors/track, 481 cylinders
Units = cylinders of 16065 * 512 = 8225280 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes
Disk identifier: 0x46e28938
Device Boot Start End Blocks Id System
/dev/sdc1 1 122 979933+ 6 FAT16
Command (m for help): a
Partition number (1-4): 1
Command (m for help): n
Command action
e extended
p primary partition (1-4)
p
Partition number (1-4): 2
First cylinder (123-481, default 123):
Using default value 123
Last cylinder, +cylinders or +size{K,M,G} (123-481, default 481):
Using default value 481
Command (m for help): p
Disk /dev/sdc: 3963 MB, 3963617280 bytes
255 heads, 63 sectors/track, 481 cylinders
Units = cylinders of 16065 * 512 = 8225280 bytes
Sector size (logical/physical): 512 bytes / 512 bytes
I/O size (minimum/optimal): 512 bytes / 512 bytes
Disk identifier: 0x46e28938
Device Boot Start End Blocks Id System
/dev/sdc1 * 1 122 979933+ 6 FAT16
/dev/sdc2 123 481 2883667+ 83 Linux
Command (m for help): w
The partition table has been altered!
Calling ioctl() to re-read partition table.
WARNING: If you have created or modified any DOS 6.x
partitions, please see the fdisk manual page for additional
information.
Syncing disks.
honey@honey-desktop:~$
honey@honey-desktop:~$
honey@honey-desktop:~$
honey@honey-desktop:~$ sudo mkdosfs -F 16 -n boot /dev/sdc1
mkdosfs 3.0.7 (24 Dec 2009)
honey@honey-desktop:~$ sudo mkfs.ext3 -L filesys /dev/sdc2
mke2fs 1.41.11 (14-Mar-2010)
warning: 20 blocks unused.
Filesystem label=filesys
OS type: Linux
Block size=4096 (log=2)
Fragment size=4096 (log=2)
Stride=0 blocks, Stripe width=0 blocks
180576 inodes, 720896 blocks
36045 blocks (5.00%) reserved for the super user
First data block=0
Maximum filesystem blocks=738197504
22 block groups
32768 blocks per group, 32768 fragments per group
8208 inodes per group
Superblock backups stored on blocks:
32768, 98304, 163840, 229376, 294912
Writing inode tables: done
Creating journal (16384 blocks): done
Writing superblocks and filesystem accounting information: done
This filesystem will be automatically checked every 39 mounts or
180 days, whichever comes first. Use tune2fs -c or -i to overrid
Then I have copied MLO, uboot and uImage in order to boot partition. And I have made adjustments to SW4 switch to be able to boot from the SD card.
Tried to boot from SD card. But No print is seen on the minicom terminal. (Neither uboot is up).
I have checked in my forums, tried out various combinations, made the boot partition as W95 Fat16, W95 Fat32 etc. But neither of the option works.
I am using Kingston 4GB SD card.
Please help me find solution to my issue.
Thanks,
Honey S