Part Number: TDA4VEN-Q1
Hi,
I noticed that there is an option for output format in the LDC node. I was wondering, if my input image format is UYVY, can the output image format be NV12? Would this cause any issues with the image?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA4VEN-Q1
Hi,
I noticed that there is an option for output format in the LDC node. I was wondering, if my input image format is UYVY, can the output image format be NV12? Would this cause any issues with the image?
Hi,
Yes, LDC does support YUV422 (UYVY) format as input and can convert it into NV12 output format.
Regards,
Brijesh
Hi enrui,
LDC H/W can do 422 to 420 conversion.
Please refer to the "Valid input/output format combinations" table below.