This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

beagle bone kernel compiling



Hi, I'm tring to rebuild kernel to beaglebone board.

Host machine have Ubuntu OS.

I use this link http://software-dl.ti.com/dsps/dsps_public_sw/am_bu/sdk/AM335xSDK/latest/exports/am335x-evm-sdk-src-05.03.03.00.tar.gz
to download the kernel source tree.

I have installed arm-linux-gnueabi- tools from Ubuntu repository using apt-get.

# make ARCH=arm CROSS_COMPILE=arm-linux-gnueabi- mrproper
# make ARCH=arm CROSS_COMPILE=arm-linux-gnueabi-
# make ARCH=arm CROSS_COMPILE=arm-linux-gnueabi- am335x_evm_defconfig
# make ARCH=arm CROSS_COMPILE=arm-linux-gnueabi- menuconfig
# make ARCH=arm CROSS_COMPILE=arm-linux-gnueabi- uImage

Boot logs are:

## Booting kernel from Legacy Image at 80007fc0 ...
   Image Name:   Linux-3.1.0
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2871008 Bytes = 2.7 MiB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
   XIP Kernel Image ... OK
OK

Starting kernel ...

Uncompressing Linux... done, booting the kernel.
[    0.071311] omap_l3_smx omap_l3_smx.0: couldn't find resource
[    0.176277] Could not set LED4 to fully on
[    0.274785] mtdoops: mtd device (mtddev=name/number) must be supplied
[    0.354210] omap2_set_init_voltage: Fail set voltage-dpll_mpu_ck(f=500000000 v=1100000)on vddmpu
[    0.363512] omap2_set_init_voltage: unable to set vdd_mpu
[    0.483528] Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(179,2)
[    0.492404] Backtrace:
[    0.495059] [<c00178c8>] (dump_backtrace+0x0/0x10c) from [<c03c648c>] (dump_stack+0x18/0x1c)
[    0.503949]  r6:c053b21c r5:00000000 r4:c05a00e0 r3:c056a290
[    0.509933] [<c03c6474>] (dump_stack+0x0/0x1c) from [<c03c66bc>] (panic+0x64/0x188)
[    0.518012] [<c03c6658>] (panic+0x0/0x188) from [<c0512c58>] (mount_block_root+0x178/0x22c)
[    0.526819]  r3:cfa4c400 r2:00000000 r1:cf81bf50 r0:c048e340
[    0.532790]  r7:00008001
[    0.535480] [<c0512ae0>] (mount_block_root+0x0/0x22c) from [<c0512ebc>] (mount_root+0xc4/0xe4)
[    0.544560] [<c0512df8>] (mount_root+0x0/0xe4) from [<c0513048>] (prepare_namespace+0x16c/0x1c4)
[    0.553809]  r4:c059f160
[    0.556484] [<c0512edc>] (prepare_namespace+0x0/0x1c4) from [<c05128c4>] (kernel_init+0xf0/0x11c)
[    0.565826]  r5:c05492a8 r4:c05492a8
[    0.569616] [<c05127d4>] (kernel_init+0x0/0x11c) from [<c0040e28>] (do_exit+0x0/0x6a8)
[    0.577952]  r5:c05127d4 r4:00000000

Thanks in advance