Part Number: J784S4XEVM
Other Parts Discussed in Thread: TDA4VH, TCA6408
We are evaluating the Lilliput TK1330-NP/C/T (13.3", 1920x1080, HDMI Capacitive Touchscreen Monitor) for use with the TI J784S4 EVM platform.
Could you please help us with the following:
- Is the Lilliput TK1330-NP/C/T touchscreen display compatible with the TI J784S4 EVM?
- If compatible:
- Are there any specific display or touch drivers required?
- Is touchscreen functionality supported on the TI Linux SDK out of the box, or are additional drivers/configurations needed?
- Could you provide any available documentation, driver packages, or display bring-up guidelines?
- If this display is not compatible or not recommended:
- Could you suggest alternative DP touchscreen displays that are known to work with the TI J784S4 EVM?
- Please share any validated display models along with the corresponding driver/support information.
Our primary requirements are:
- DP display interface
- 1920x1080 resolution
- Capacitive touch support
- Linux SDK compatibility on J784S4 EVM