Other Parts Discussed in Thread: TMS320C5515, PCM3168
I'm looking at an application for the TMS320C5515 where I need to ingest at least 4 channels of audio data. I'm hoping I can use a 4 or more channel codec such as the pcm3168 or AK5388. From what I can tell, the I2S controller in the C5515 only directly supports stereo audio. Is there a way to configure the controller to support a multichannel TDM I2S signal such as that provided by the pcm3168? Barring this I will use 2 stereo codecs and share the clock signals between them with one codec in master mode and all other devices in slave mode to achieve concurrent sampling.