Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Verified DDR3 chip

Dear Sir :

        Is there Verified DDR3 part Number ?

        thanks

gfeathers

  • Hi all,

    I'm facing the same issue using an DDR3 memory with an AM335x.

    Is there a verified DDR3 memory available? Or can I use any DDR3 device, which is e.g. DDR-1066 compatible, using it with 303MHz clock (for example an Micron device MT41J256M8)?

    Thanks for you help!

    FNCR / S.I.E