Part Number: AM62A7
Hello Team,
We are using AM62A7 starter kit, 11.01.07.05 version of edgeai linux sdk. While running vision_apps_init.sh we are getting the following error
root@am62axx-evm:/opt/vision_apps# source ./vision_apps_init.sh
root@am62axx-evm:/opt/vision_apps# 0.000000 s: APP_LOG: ERROR: Unable to map memory @ 0xa1000000 of size 262144 bytes !!!
APP_LOG: ERROR: Unable to map memory @ 0xa2000000 of size 3288576 bytes !!!
The same error comes up when we are trying to run https://github.com/TexasInstruments-Sandbox/edgeai-rgb-ir-app-examples/blob/main/gstreamer-pipelines/gst-command-rgb-display.sh
So, we feel some memory mapping is not done correctly in OpenVx. This is a fresh sdk installed and done make and flashed to sd card. Please help us with the issue.
Thank you