This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6424 EMAC driver potential BUG

Hello


i am connection 2 c6424 EVMs back to back (thorugh the ethernet) (EvmA, EvmB)

Trafiic is flowing OK - voice is passing fine between the EVM.

I am doint the follwing:

1. Disconnecting power of EvmB and reconnecting. --> traffic is back.

But... sometimes there is a problem in the Phy/MDIO - traffic stops to flow. Then I disconnect the Eth cable, but MDIO registers shows that there is still link.

This is a bug.

 

As far as I understand - the MDIO polls indnependly the register from the PHY, there is no DSP/SW involvment in it so it is not the EMAC driver error.

 

Anyone had this before?

Any leads how to solve it?

 

Yoav