This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Execution time with device Simulator of DM6437

Hello,

I'm working with the device simulator of DM6437 on CCS v5.1 and i did a small application with C6FLo which makes a MedianFilter on a set of data.

Everythings seem to works since i get a correct output but now i will evaluate the real time needed to process the median filter in order to benchmarking the application.

I've no idea how to do that. Here is a picture with the LOG_printf output and CPU load graph.

 

I tried to put a Log-printf before and after the call of the median filter for exemple on this picture time 3 and 4.( Do not pay attention to the time 2 with the error). 

So what is the unit of time in Log-printf? It's seem that there is only one time unit to process the median filter??????? It's not possible.

How to get the real time?

On the cpu load graph the time is in "ns" is it true time?

I set the clock speed of the CPU to 600MHz in the ccxml and tcf file.

Thank you for your help.