Part Number: J722SXH01EVM
Other Parts Discussed in Thread: AM67
I have installed the CCS version 21.0.0 on my Ubuntu laptop and trying to connect and debug code on a J722S EVM.
I am trying to follow the instructions on https://software-dl.ti.com/ccs/esd/documents/users_guide_ccs_21.0.0/ccs_getting-started.html to get started with running a simple program on the EVM, specifically on one of the DSPs. I followed section 4.4.1 to create a new empty project for the C7x core and then tried to run the program on the target following the steps in section 4.5. While loading the program, I get these errors:
C75X_0: File Loader: Verification failed: Values at address 0x0000000000002018 do not match (expected: 0x40, actual: 0x00) Please verify target memory and memory map.
C75X_0: GEL: File: /home/aparna/workspace_ccstheia/MyTry/Debug/MyTry.out: a data verification error occurred, file load failed.
The above errors are with the DIP switches set to SD-card boot. Do we need some GEL files to do the proper initialization before loading ? I could not locate any GEL files for this EVM in the CCS folder.
On setting the boot-switches to No-boot mode, I am getting this error on trying to load and debug the program.
CS_DAP_0: Error connecting to the target: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 21.0.0.3955)
Please suggest the right sequence of steps to be able to run and load a stand-alone program on the DSPs.
Regards,
Aparna