This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

H264 bitrate is out of control

Hi All:

As we know the maximum bitrate for H264 Baseline profile level 3.1 is up to 14Mbps(From ISO/IEC 14496 A-1), I have tried use DM365 to encode H264 Baseline profile level 3.1 streams under Fix Qp mode, and I found that the release bitrate can reach to 25Mbps under some special scene, is this reasonable from the standard? Is there any way to control this? Thanks.