This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA821U: Invalid values generated by syscfg for DRA821

Part Number: DRA821U

Hi, I've been using web sysfscg to configure my board, and looking at the generated devicetree.dtsi it points to symbols that are not available in the SDK (11.0.0.4). E.g. 

	gpio_pins_default: gpio-default-pins {
		pinctrl-single,pins = <
			J7200_IOPAD(0x03c, PIN_INPUT, 7) /* (W16) MCAN3_RX.GPIO0_16 */
			J7200_IOPAD(0x048, PIN_INPUT, 7) /* (V21) MCAN5_TX.GPIO0_19 */
			J7200_IOPAD(0x070, PIN_INPUT, 7) /* (U17) MCAN10_TX.GPIO0_29 */
			J7200_IOPAD(0x074, PIN_INPUT, 7) /* (U20) MCAN10_RX.GPIO0_30 */
			J7200_IOPAD(0x0a4, PIN_INPUT, 7) /* (W14) UART8_RXD.GPIO0_42 */
			J7200_IOPAD(0x0a8, PIN_INPUT, 7) /* (W19) UART8_TXD.GPIO0_43 */
			J7200_IOPAD(0x0b0, PIN_INPUT, 7) /* (T16) UART0_RXD.GPIO0_47 */
		>;
	};

J7200_IOPAD is not avaiable in the SDK uboot / linux source code. I see that J721E_* symbols are available and used even on J7200 SoC but the fact that syscfg generates invalid entries is at least confusing.