This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62L: AM62L KeyWriter Lite failed

Part Number: AM62L

Hi,

I'm trying to write the e-fuses in an AM62L to provision an SMPK and other OTP values, but am getting a generic error back from the TISCI without any details on what is wrong.

Steps I've followed so far:

  1. Generate the keywriter lite blob using the key configurator from here: https://github.com/TexasInstruments/security-utils/tree/release/key_configurator
  2. My configuration uses multi-shot mode, and enables the mpkopts, smpkh, keycnt, keyrev, sblswrev, sysfwswrev and brdcfgswrev fields. All other fields are not enabled. I've attached the generated .c and .bin files (zipped: keywrlite.zip )
  3. Try to write the blob following the instructions from here (with the only change being that we're using our own hardware, so the Vpp pin 1V8 supply is enabled by other means than the I2C GPIO described in the document): https://software-dl.ti.com/processor-sdk-linux/esd/AM62LX/latest/exports/docs/linux/Foundational_Components/U-Boot/UG-Key-Writer-Lite.html

This just results in a non-specific error code, the whole log of the u-boot console is below:

=> mw 0x82000000 0 0x400
=> load mmc 0:1 0x82000000 keywrlite.bin
636 bytes read in 1 ms (621.1 KiB/s)
=> dcache flush
=> md 0x82000000
82000000: 00000001 00009045 02209012 00000100  ....E..... .....
82000010: 00000001 00000000 00000000 00004a7e  ............~J..
82000020: a5a5a55a 00000000 00000000 00000000  Z...............
82000030: 00001234 5aa5a55a d87a1a6d 29f073a4  4...Z..Zm.z..s.)
82000040: ff3cf0c5 29b4cc00 25e25355 d49f83b5  ..<....)US.%....
82000050: 9e80bdbe 731a3fc1 3f7374ba 06df222b  .....?.s.ts?+"..
82000060: 40f13938 57b19b9f e458e874 6127c1b2  89.@...Wt.X...'a
82000070: 16e82171 751aa386 00000000 00000000  q!.....u........
82000080: 00009ffc a5a5a5a5 00000000 00000000  ................
82000090: 00000000 00000000 00000000 00000000  ................
820000a0: 00000000 00000000 00000000 00000000  ................
820000b0: 00000000 00000000 00000000 00000000  ................
820000c0: 00000000 00000000 00000000 00000000  ................
820000d0: 00005678 a5a5a55a 00000001 00000000  xV..Z...........
820000e0: 00000000 000062c8 a5a5a55a 00000001  .....b..Z.......
820000f0: 00000000 00000000 00008bad a5a5a55a  ............Z...
=> fuse writebuff -y 0x82000000
Programming fuses using a structured buffer in memory starting at addr 0x82000000
NOTICE:  Writebuff version info: 0x1
ERROR:   Failed to get response (-19)
ERROR:   Transfer send failed (-19)
ERROR:   Keywriter Lite Failed: (-19)
SMC call failed: Error code -1
ERROR
=> 

Based on this thread: https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1641521/am62l-am62l-secure-boot-keywriter-lite it seems possible to get logs from TISCI over WKUP_UART0, so I followed the same steps (set trace_dst_enables: 0x01 and trace_src_enables: 0x1F in board-cfg.yaml in the u-boot repo), but there is no output on WKUP_UART0 when attempting the key write. Are these config values documented somewhere? What is the baud rate of the UART (I assumed 115200)?

Tracing the error messages back through the TF-A source code, it seems like the TISCI does not ACK the message in the event that anything is wrong.

I'd like to re-iterate the comment in here https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1578568/am62l-am62l-secure-boot-keywriter-lite that I would expect some kind of useful error code from TISCI to help figure out the problem rather than just ignoring the message entirely.

Is there anything else you recommend to debug what the problem is here? Is the keywriter lite blob itself correct?

Thanks

Matt

  • Hi Matt,
    Which Linux SDK version was used in your testing?
    Best,
    -Hong

  • Hi Hong,

    We're not using the SDK directly, instead we have our own yocto build which is building u-boot, tispl and tiboot3 from a fork of the upstream repo: https://github.com/TexasInstruments/ti-u-boot with support for our own board added. Our branch is forked from the ti-u-boot-2025.01 branch in late 2025.

    Is there a specific commit or set of commits that I should check are included in our branch to fully support keywriter lite?

    Thanks

    Matt

  • Hi Matt,
    Let me run some testing on my side, and get back to you.
    Best,
    -Hong

  • Hi Matt,

    I analysed the key blob you generated.
    On AM62L SoC, the three SWRV for SBL/SYSFW/BRDCFG are pre-programmed as "1" at TI Fab.
    These're two options:
    - remove the three SWRV fields when generating the key blob
    - activate the "override" action flag when inlcuding the three SWRV fields in the key blob

    I'm attaching the u-boot patch to enable TIFS trace on WKUP_UART0, and I'm able to capture the TIFS trace on TI AM62L EVM.

    Best,
    -Hong

    https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/791/am62l_5F00_tifs_5F00_trace.patch

  • Hi Hong,

    Thanks, this is working now when I disable writing the three SWREV fields.

    One more question - is there a precise specification of exactly what should be hashed to get the SMPKH (or BMPKH) value to write to OTP?

    I checked the source code of the python key_configurator in TI's security-utils repo and it hashes the entire DER file given to it. So I'm assuming that the DER file given to the tool should contain only a SubjectPublicKeyInfo structure, and the TI secure ROM hashes the same SubjectPublicKeyInfo structure that's contained in the x509 certificate for tiboot3.bin and tispl.bin for comparison?

    Can you confirm if this is correct (or point out somewhere this is already documented if I've missed it)?

    Thanks

    Matt

  • Hi Matt,
    Yes, your understanding is correct.
    It looks like this with the TI testing key as an example
    $ openssl sha512 smpk_public.der
    SHA512(smpk_public.der)= 1f6002b07cd9b0b7c47d9ca8d1aae57b8e8784a12f636b2b760d7d98a18f189760dfd0f23e2b0cb10ec7edc7c6edac3d9bdfef
    Best,
    -Hong