Part Number: TMS570LC4357
A 24-bit external ADC is connected to the TMS570LC4357 SPI3 line to read sensor data within the circuit. I am reading differential and single-ended data from this external ADC. I am getting errors in the data I am reading. The differential data I am reading is -2^15 (-32768), and the single-ended data I am reading is 2^7 (127). I have 3 circuits with this design in my system. I do not experience this problem in 2 circuits. I experience it in 1 circuit. And this fault is not a constant fault. It comes and goes on its own in a short time. When I measured the SPI line, I did not see any overshoot or ringing.