Other Parts Discussed in Thread: SYSBIOS
Hello Gents,
We are trying to bring EMAC interface UP and RUNNING on our own hardware. We have a code compiling and running well on the DSK6455. We are trying to troubleshoot what appears to be a MDIO issue. The EMAC/MDIO connections are routed through an FPGA and we are trying to verify the MDIO protocol itself.
We have two different issues, the first one being "NO_PHY_DETECTED" and I can fairly understand why and so on. The second one a bit more difficult is NDK not calling HwPktPoll() at all. I was hoping to read from experienced engineers what could actually make NDK not to POLL anymore, is there anything obvious I could check? I am surprised we are getting either NO_PHY_CONNECTED or no poll at all. The NO_PHY_CONNECTED error is thrown by _HwPktPoll() which indicates in these circumstance the function is called by NDK.
Best Regards,
Arnaud