Part Number: DP83TG721EVM-MC
Other Parts Discussed in Thread: AM62A7,
We are working on AM62A7 based custom board with TJA1120A Auto Ethernet PHY.
We connected DP83TG721EVM-MC AutoEthernet to our Custom Board. Link was detected.
root@am62axx-evm:~# dmesg | grep eth
[ 0.000000] psci: probing for conduit method from DT.
[ 0.944429] optee: probing for conduit method.
[ 1.352845] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA01103, cpsw version 0x6BA81103 Ports: 3 quirks:00000006
[ 1.365779] am65-cpsw-nuss 8000000.ethernet: Use random MAC address
[ 1.452604] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.5
[ 1.459737] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512, Policers 32
[ 1.467615] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:1
[ 1.488042] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 19
[ 5.875382] am65-cpsw-nuss 8000000.ethernet eth1: PHY [8000f00.mdio:00] driver [Micrel KSZ9031 Gigabit PHY] (irq=POLL)
[ 5.890378] am65-cpsw-nuss 8000000.ethernet eth1: configuring for phy/rgmii link mode
[ 6.618291] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:04] driver [NXP C45 TJA1120] (irq=POLL)
[ 6.629693] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii link mode
[ 6.662963] am65-cpsw-nuss 8000000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off
[ 38.194116] am65-cpsw-nuss 8000000.ethernet eth0: Link is Down
[ 116.023614] am65-cpsw-nuss 8000000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off
Right now Media Converter is set to Slave and TJA1120 to Master. Media Converter in Autonomous mode.
root@am62axx-evm:~# ethtool eth0
Settings for eth0:
Supported ports: [ TP MII ]
Supported link modes: 1000baseT1/Full
Supported pause frame use: Symmetric
Supports auto-negotiation: No
Supported FEC modes: Not reported
Advertised link modes: 1000baseT1/Full
Advertised pause frame use: Symmetric
Advertised auto-negotiation: No
Advertised FEC modes: Not reported
Speed: 1000Mb/s
Duplex: Full
Auto-negotiation: off
master-slave cfg: forced master
master-slave status: master
Port: Twisted Pair
PHYAD: 4
Transceiver: external
MDI-X: Unknown
Supports Wake-on: d
Wake-on: d
Current message level: 0x000020f7 (8439)
drv probe link ifdown ifup rx_err tx_err hw
Link detected: yes
SQI: 7/7
FYI eth0 is the Auto-Ethernet
But ping dosent work
acs@a-tract-10:~$ ping 192.168.1.100
PING 192.168.1.100 (192.168.1.100) 56(84) bytes of data.
From 192.168.1.101 icmp_seq=1 Destination Host Unreachable
From 192.168.1.101 icmp_seq=2 Destination Host Unreachable
From 192.168.1.101 icmp_seq=3 Destination Host Unreachable
From 192.168.1.101 icmp_seq=4 Destination Host Unreachable
From 192.168.1.101 icmp_seq=5 Destination Host Unreachable
From 192.168.1.101 icmp_seq=6 Destination Host Unreachable
^C
--- 192.168.1.100 ping statistics ---
8 packets transmitted, 0 received, +6 errors, 100% packet loss, time 7185ms
pipe 4
When i Ping from my laptop, i can see LEDs on my custom board blinking. But ping dosent succeed.
root@am62axx-evm:~# ifconfig
eth0 Link encap:Ethernet HWaddr 64:1C:10:1C:06:E2
inet addr:192.168.1.100 Bcast:192.168.1.255 Mask:255.255.255.0
inet6 addr: fe80::661c:10ff:fe1c:6e2/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:84 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:16232 (15.8 KiB)
eth1 Link encap:Ethernet HWaddr E2:F1:04:D8:68:19
inet addr:192.168.2.100 Bcast:192.168.2.255 Mask:255.255.255.0
inet6 addr: fe80::e0f1:4ff:fed8:6819/64 Scope:Link
UP BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:472 errors:0 dropped:0 overruns:0 frame:0
TX packets:500 errors:0 dropped:6 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:44160 (43.1 KiB) TX bytes:57756 (56.4 KiB)
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:30 errors:0 dropped:0 overruns:0 frame:0
TX packets:30 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:3262 (3.1 KiB) TX bytes:3262 (3.1 KiB)
Kindly help us if anything more needs to be done since its Automotive ethernet and autonegotiation is not supported here.