This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM814x Supply Sequencing



Hi,

The DM814x datasheet mentions four supply Sequencing groups-

1. All CVDD supplies (CVDD, CVDD_x)
2. All 1.5-V Supplies (DVDD_DDR[x] at 1.5 V [only needed if using DDR3])
3. All 1.8-V Supplies (DVDD_x, DVDD_M, DVDD_DDR[x] at 1.8 V [if using LPDDR, DDR2], VDDA_x_1P8, VDDA_1P8)
4. All 3.3-V Supplies (DVDD, DVDD_x, DVDD_C, VDDA_x_3P3)
Also it is recommended to use PMIC TPS659113 for proper supply sequencing.

Is there any sequencing required within individual group/s?
What if all the rails are enabled simultaneously?
Where can i find more information details for supply sequencing?

   What power saving modes will be available if PMIC TPS659113 is not used?