Hi,
We are facing following error message on CCS window after application code runs.
Once we get this error, we need power cycle on EVM.
Would you tell us possible causes of the error shown below?
How can I fix this issue?
Main function comes out and SYS/BIOS started.
----
Cortex_M3_RTOS: Warning: (Error -1268 @ 0x90001)
Device is locked up in Hard Fault or in NMI. Reset the device,
and retry the operation. If error persists, confirm configuration,
power-cycle the board, and/or try more reliable JTAG settings
(e.g. lower TCLK). (Release 5.0.429.0)
SYS/BIOS started after main function comes out,
ti.sysbios.family.arm.m3.Hwi: line 801: E_hardFault: FORCED
ti.sysbios.family.arm.m3.Hwi: line 913: E_usageFault: INVSTATE
Exception occurred in background thread.
Exception occurred in ThreadType_Task.
Task handle: 0x8f100020.
Task stack base: 0x8f105600.
Task stack size: 0xff8.
R0 = 0x00000000 R8 = 0x00000000
R1 = 0x8f112510 R9 = 0xffffffff
R2 = 0x8f10c981 R10 = 0xffffffff
R3 = 0x00000000 R11 = 0xffffffff
R4 = 0x8f110d50 R12 = 0x00000090
R5 = 0x8f1125e4 SP(R13) = 0x8f112010
R6 = 0x00000001 LR(R14) = 0x8f10efcb
R7 = 0x00000010 PC(R15) = 0x00000000
PSR = 0x60000000
ICSR = 0x00000803
MMFSR = 0x00
BFSR = 0x00
UFSR = 0x0002
HFSR = 0x40000000
DFSR = 0x00000000
MMAR = 0xe000ed34
BFAR = 0xe000ed38
AFSR = 0x00000000
Terminating execution...
Regards,
Kasuya