TMDS64EVM: 32-bit GPMC Driver

Part Number: TMDS64EVM
Other Parts Discussed in Thread: SYSCONFIG

Hi Anil,

Continue to the previous problem that you recommended according to the following link :

https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1641324/tmds64evm-how-to-configure-gpmc-for-32-bit-psram-interface/6353038

The problem is after copying the files that was autogenerated and modify the files as well as disable the GPMC config is SYSCONFIG file. The build will still generate the error as : "System_Init" redefined as first already defined in ./syscfg/ti_drivers_config.o . The ti_drivers_config.c was the one to copy from autogenerated file with "GPMC" and the current ti_drivers_config.c wihout "GPMC" is autogenerated again when compiling. How to disable those autogenerated from compiling and only compiling the files that copied to the project from the beginning ?

Sorry I have to generate the new issue because the last issue the RESPONSE button was not available.

THanks,

Huynh