AM62P-Q1: Regarding the tolerable X-ray absorbed dose

Part Number: AM62P-Q1

Dear TI-Enginners,

I would like to know the X-ray absorption dose (causing temporary failure) that this component can withstand.

Q1. Is the recommended upper limit 0.1 Gy?
Q2. Please share any test results if available.

Thank you.
Junji,

  • Junji

    I am check on this and will get back to you early next week. 

    --Paul 

  • Junji

    I Received the answer quicker than expected.

    The following FAQ answer is at the bottom of the Reliability page on ti.com (https://www.ti.com/quality-reliability/reliability.html)

    Whare Can I find X-Ray sensitivity information? 

    TI does not typically specify acceptable x-ray levels on the device datasheet. Experience has shown that most TI products will NOT be sensitive to typical x-ray inspection (with typical exposures < 100 rad(Si)). X-ray exposures over these limits, however, may cause damage to the device and should be avoided.

    THIS INFORMATION IS PROVIDED "AS IS." It could change without notice. Customers are solely responsible to conduct sufficient engineering and additional qualification testing to determine whether a device is suitable for use in their applications. Using TI products outside limits stated in TI's official published Specifications may void TI's warranty. See TI's Terms of Sale for more information.

    For more information, visit our reliability testing page.