This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Android compilation aborting

Hi,

I am using Ubuntu 11.10 on a 64bit AMD Dual Core processor.

I am trying to compile the source following download : http://software-dl.ti.com/dsps/dsps_public_sw/sdo_tii/TI_Android_DevKit/TI_Android_GingerBread_2_3_4_DevKit_2_1/exports/TI_Android_GingerBread_2_3_4Sources.tar.gz

I am following instructions on : http://processors.wiki.ti.com/index.php/TI-Android-GingerBread-2.3.4-DevKit-2.1_DeveloperGuide

Everything seems to be going fine, until I try to make the Android platform using the following shell command line : make TARGET_PRODUCT=omap3evm OMAPES=5.x -j4

I am getting the following error:

============================================
PLATFORM_VERSION_CODENAME=REL
PLATFORM_VERSION=2.3.4
TARGET_PRODUCT=omap3evm
TARGET_BUILD_VARIANT=eng
TARGET_SIMULATOR=
TARGET_BUILD_TYPE=release
TARGET_BUILD_APPS=
TARGET_ARCH=arm
HOST_ARCH=x86
HOST_OS=linux
HOST_BUILD_TYPE=release
BUILD_ID=GRJ22
============================================
find: `frameworks/base/frameworks/base/docs/html': No such file or directory
find: `out/target/common/docs/gen': No such file or directory
find: `frameworks/base/frameworks/base/docs/html': No such file or directory
find: `out/target/common/docs/gen': No such file or directory
find: `frameworks/base/frameworks/base/docs/html': No such file or directory
find: `out/target/common/docs/gen': No such file or directory
find: `frameworks/base/frameworks/base/docs/html': No such file or directory
find: `out/target/common/docs/gen': No such file or directory
find: `frameworks/base/frameworks/base/docs/html': No such file or directory
find: `out/target/common/docs/gen': No such file or directory
*** glibc detected *** make: free(): invalid next size (fast): 0x0000000006d84950 ***
======= Backtrace: =========
/lib/x86_64-linux-gnu/libc.so.6(+0x78a96)[0x7f81b7a62a96]
/lib/x86_64-linux-gnu/libc.so.6(cfree+0x6c)[0x7f81b7a66d7c]
make[0x40a7da]
make[0x40cb4b]
make[0x40784b]
make[0x40734b]
make[0x4073f3]
make[0x40cb14]
make[0x40784b]
make[0x40734b]
make[0x407540]
make[0x407c92]
make[0x40b844]
make[0x40cb4b]
make[0x40784b]
make[0x40734b]
make[0x41d5aa]
make[0x41dc2b]
make[0x416088]
make[0x4175e2]
make[0x4167f6]
make[0x4175e2]
make[0x4179ac]
make[0x4033d3]
/lib/x86_64-linux-gnu/libc.so.6(__libc_start_main+0xed)[0x7f81b7a0b30d]
make[0x40420d]
======= Memory map: ========
00400000-00429000 r-xp 00000000 08:06 21005                              /usr/local/bin/make
00628000-00629000 r--p 00028000 08:06 21005                              /usr/local/bin/make
00629000-0062b000 rw-p 00029000 08:06 21005                              /usr/local/bin/make
0062b000-0062c000 rw-p 00000000 00:00 0
008af000-06f64000 rw-p 00000000 00:00 0                                  [heap]
7f81b0000000-7f81b0021000 rw-p 00000000 00:00 0
7f81b0021000-7f81b4000000 ---p 00000000 00:00 0
7f81b6dd2000-7f81b6de7000 r-xp 00000000 08:06 4827                       /lib/x86_64-linux-gnu/libgcc_s.so.1
7f81b6de7000-7f81b6fe6000 ---p 00015000 08:06 4827                       /lib/x86_64-linux-gnu/libgcc_s.so.1
7f81b6fe6000-7f81b6fe7000 r--p 00014000 08:06 4827                       /lib/x86_64-linux-gnu/libgcc_s.so.1
7f81b6fe7000-7f81b6fe8000 rw-p 00015000 08:06 4827                       /lib/x86_64-linux-gnu/libgcc_s.so.1
7f81b6fe8000-7f81b70e9000 rw-p 00000000 00:00 0
7f81b70e9000-7f81b77cd000 r--p 00000000 08:06 136751                     /usr/lib/locale/locale-archive
7f81b77cd000-7f81b77e5000 r-xp 00000000 08:06 4866                       /lib/x86_64-linux-gnu/libpthread-2.13.so
7f81b77e5000-7f81b79e4000 ---p 00018000 08:06 4866                       /lib/x86_64-linux-gnu/libpthread-2.13.so
7f81b79e4000-7f81b79e5000 r--p 00017000 08:06 4866                       /lib/x86_64-linux-gnu/libpthread-2.13.so
7f81b79e5000-7f81b79e6000 rw-p 00018000 08:06 4866                       /lib/x86_64-linux-gnu/libpthread-2.13.so
7f81b79e6000-7f81b79ea000 rw-p 00000000 00:00 0
7f81b79ea000-7f81b7b7f000 r-xp 00000000 08:06 4806                       /lib/x86_64-linux-gnu/libc-2.13.so
7f81b7b7f000-7f81b7d7e000 ---p 00195000 08:06 4806                       /lib/x86_64-linux-gnu/libc-2.13.so
7f81b7d7e000-7f81b7d82000 r--p 00194000 08:06 4806                       /lib/x86_64-linux-gnu/libc-2.13.so
7f81b7d82000-7f81b7d83000 rw-p 00198000 08:06 4806                       /lib/x86_64-linux-gnu/libc-2.13.so
7f81b7d83000-7f81b7d89000 rw-p 00000000 00:00 0
7f81b7d89000-7f81b7d90000 r-xp 00000000 08:06 4870                       /lib/x86_64-linux-gnu/librt-2.13.so
7f81b7d90000-7f81b7f8f000 ---p 00007000 08:06 4870                       /lib/x86_64-linux-gnu/librt-2.13.so
7f81b7f8f000-7f81b7f90000 r--p 00006000 08:06 4870                       /lib/x86_64-linux-gnu/librt-2.13.so
7f81b7f90000-7f81b7f91000 rw-p 00007000 08:06 4870                       /lib/x86_64-linux-gnu/librt-2.13.so
7f81b7f91000-7f81b7fb2000 r-xp 00000000 08:06 4793                       /lib/x86_64-linux-gnu/ld-2.13.so
7f81b808e000-7f81b8192000 rw-p 00000000 00:00 0
7f81b81a3000-7f81b81aa000 r--s 00000000 08:06 267343                     /usr/lib/x86_64-linux-gnu/gconv/gconv-modules.cache
7f81b81aa000-7f81b81ab000 rw-p 00000000 00:00 0
7f81b81ad000-7f81b81b1000 rw-p 00000000 00:00 0
7f81b81b1000-7f81b81b2000 r--p 00020000 08:06 4793                       /lib/x86_64-linux-gnu/ld-2.13.so
7f81b81b2000-7f81b81b4000 rw-p 00021000 08:06 4793                       /lib/x86_64-linux-gnu/ld-2.13.so
7fff98ef6000-7fff98f2b000 rw-p 00000000 00:00 0                          [stack]
7fff98f90000-7fff98f91000 r-xp 00000000 00:00 0                          [vdso]
ffffffffff600000-ffffffffff601000 r-xp 00000000 00:00 0                  [vsyscall]
Aborted

At first I thought that this line [*** glibc detected *** make: free(): invalid next size (fast): 0x0000000006d84950 *** ] meant that I had too little memory to compile successfully. I then bought and installed 8Gb of memory but I got the same error.

Please help,