This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can the DM3725 DDR controller use two 32-bit data DDR ICs connected in a T-connection style?



I do not see any mention of it in the literature.  I see only 2 16 bit DDRs or a single 32 bit DDR.  We are trying to do this and it is not exactly clear what rules should be followed for this.  Also the pinout on the CUS package for this type of routing is not optimal.  I am hoping to get some thoughts on this.