This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

On the run on DM642 NDK, DHCPS service can not start problem

I meet a problem, use DM642 evaluation board, running NDK, DHCP Server can't start, the program to run after the report returns to failed, Telnet, HTTP start, I tested NDK1.7, NDK1.9, NDK2.0, are the same results, test procedures for NDK routines ( in NDK2.0 there is complete without need to modify the routine), running environment based on datasheet to illustrate the use of the newer version. Compiler program without error, ccs3.3.81, CGT6.1.16, BIOS5.41.55. May I ask what is the place of issue? DM642 does not support DHCP Server? Or give tips may be where the problem is? Thank you thank you thank you