This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62L-EVSE-DEV-EVM: AM62AX-EVM-K3R5: Yocto build fails : do_deploy_setscene

Hi Vinuchandran,

Thankyou for the reply.

The issue was fixed once we downgraded tar package.

Now I am facing some errors build. Is this related to previous failed build?


ERROR: tisdk-uenv-1.0-r3_tisdk_1 do_deploy_setscene: Recipe tisdk-uenv is trying to install files into a shared area when those files already exist. The files and the manifests listing them are:
/home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/uEnv.txt
(not matched to any task)
Please adjust the recipes so only one recipe provides a given file.
ERROR: optee-ftpm-git-r0 do_deploy_setscene: Recipe optee-ftpm is trying to install files into a shared area when those files already exist. The files and the manifests listing them are:
/home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/optee/bc50d971-d4c9-42c4-82cb-343fb7f37896.stripped.elf
(not matched to any task)
Please adjust the recipes so only one recipe provides a given file.
WARNING: Logfile for failed setscene task is /home/vysakh2/MNMI_SVSC/tisdk/build/arago-tmp-default-glibc/work/am62axx_evm-oe-linux/optee-ftpm/git/temp/log.do_deploy_setscene.554565
WARNING: Logfile for failed setscene task is /home/vysakh2/MNMI_SVSC/tisdk/build/arago-tmp-default-glibc/work/am62axx_evm-oe-linux/tisdk-uenv/1.0/temp/log.do_deploy_setscene.554570
WARNING: Setscene task (/home/vysakh2/MNMI_SVSC/tisdk/sources/meta-arago/meta-arago-distro/recipes-tisdk/tisdk-uenv/tisdk-uenv.bb:do_deploy_setscene) failed with exit code '1' - real task will be run instead
WARNING: Setscene task (/home/vysakh2/MNMI_SVSC/tisdk/sources/meta-arm/meta-arm/recipes-security/optee-ftpm/optee-ftpm_git.bb:do_deploy_setscene) failed with exit code '1' - real task will be run instead
ERROR: ti-dm-fw-11.01.09-r4.0 do_deploy_setscene: Recipe ti-dm-fw is trying to install files into a shared area when those files already exist. The files and the manifests listing them are:
/home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/ti-dm/am62axx/dm_edgeai_mcu1_0_release_strip.out.signed
(not matched to any task)
/home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/ti-dm/am62axx/dm_edgeai_mcu1_0_release_strip.out
(not matched to any task)
Please adjust the recipes so only one recipe provides a given file.
WARNING: Logfile for failed setscene task is /home/vysakh2/MNMI_SVSC/tisdk/build/arago-tmp-default-glibc/work/am62axx_evm-oe-linux/ti-dm-fw/11.01.09/temp/log.do_deploy_setscene.554567
WARNING: Setscene task (/home/vysakh2/MNMI_SVSC/tisdk/sources/meta-ti/meta-ti-bsp/recipes-bsp/ti-dm-fw/ti-dm-fw.bb:do_deploy_setscene) failed with exit code '1' - real task will be run instead
ERROR: trusted-firmware-a-2.13+git-r0 do_deploy_setscene: Recipe trusted-firmware-a is trying to install files into a shared area when those files already exist. The files and the manifests listing them are:
/home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/bl31.elf
(not matched to any task)
/home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/bl31-k3.elf
(not matched to any task)
/home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/bl31-k3.bin
(not matched to any task)
/home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/bl31.bin
(not matched to any task)
Please adjust the recipes so only one recipe provides a given file.
WARNING: Logfile for failed setscene task is /home/vysakh2/MNMI_SVSC/tisdk/build/arago-tmp-default-glibc/work/am62axx_evm-oe-linux/trusted-firmware-a/2.13+git/temp/log.do_deploy_setscene.554569
WARNING: Setscene task (/home/vysakh2/MNMI_SVSC/tisdk/sources/meta-arm/meta-arm/recipes-bsp/trusted-firmware-a/trusted-firmware-a_2.10.4.bb:do_deploy_setscene) failed with exit code '1' - real task will be run instead
ERROR: optee-os-4.6.0+git-r0_tisdk_6 do_deploy_setscene: Recipe optee-os is trying to install files into a shared area when those files already exist. The files and the manifests listing them are:
/home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/bl32.bin
(not matched to any task)
/home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/bl32.elf
(not matched to any task)
/home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/optee/tee-pageable_v2.bin
(not matched to any task)
/home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/optee/bl32.bin
(not matched to any task)
/home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/optee/tee-raw.bin
(not matched to any task)
/home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/optee/tee-pager_v2.bin
(not matched to any task)
/home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/optee/tee.elf
(not matched to any task)
/home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/optee/tee-header_v2.bin
(not matched to any task)
/home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/optee/bl32.elf
(not matched to any task)
/home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/optee/tee.bin
(not matched to any task)
/home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/optee/ta/fd02c9da-306c-48c7-a49c-bbd827ae86ee.stripped.elf
(not matched to any task)
/home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/optee/ta/f04a0fe7-1f5d-4b9b-abf7-619b85b4ce8c.stripped.elf
(not matched to any task)
/home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/optee/ta/80a4c275-0a47-4905-8285-1486a9771a08.elf
(not matched to any task)
/home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/optee/ta/023f8f1a-292a-432b-8fc4-de8471358067.stripped.elf
(not matched to any task)
/home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/optee/ta/f04a0fe7-1f5d-4b9b-abf7-619b85b4ce8c.elf
(not matched to any task)
/home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/optee/ta/fd02c9da-306c-48c7-a49c-bbd827ae86ee.elf
(not matched to any task)
/home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/optee/ta/80a4c275-0a47-4905-8285-1486a9771a08.stripped.elf
(not matched to any task)
/home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/optee/ta/023f8f1a-292a-432b-8fc4-de8471358067.elf
(not matched to any task)
Please adjust the recipes so only one recipe provides a given file.

can you find the solution for this error?


  • Split from  AM62L-EVSE-DEV-EVM: AM62AX-EVM-K3R5: Yocto build fails in linux-firmware:do_package with pseudo errors (Cannot mkdir: Bad address) 

    Hi,

    This is a classic Yocto sstate/deploy-manifest desync, and given the timing, it's very likely a direct consequence of the earlier pseudo corruption.

    Try clearing the machine's entire deploy output and let sstate regenerate it cleanly:

    rm -rf build/deploy-ti/images/am62axx-evm/*
    bitbake -c cleansstate tisdk-uenv optee-ftpm ti-dm-fw trusted-firmware-a optee-os
    bitbake <your-image>

    Regards,
    Vinu

  • Hi Vinuchandran,

    Thank you for the quick reply.

    I am facing this issue after removing files inside am62axx-evm

    ERROR: tisdk-default-image-1.0-r0_tisdk_5 do_image_wic: ExecutionError('/home/vysakh2/MNMI_SVSC/tisdk/build/arago-tmp-default-glibc/work/am62axx_evm-oe-linux/tisdk-default-image/1.0/temp/run.do_image_wic.579554', 1, None, None)
    ERROR: Logfile of failure stored in: /home/vysakh2/MNMI_SVSC/tisdk/build/arago-tmp-default-glibc/work/am62axx_evm-oe-linux/tisdk-default-image/1.0/temp/log.do_image_wic.579554

  • Hi,

    That top-level ExecutionError is just BitBake's wrapper. It only tells you the wic task failed and where the log lives, not why.

    The actual root cause will be in the last ~30-50 lines of /home/vysakh2/MNMI_SVSC/tisdk/build/arago-tmp-default-glibc/work/am62axx_evm-oe-linux/tisdk-default-image/1.0/temp/log.do_image_wic.579554

    Please share it.

    Regards,
    Vinu

  • Hi Vinuchandran,

    Please find the logs

    DEBUG: Executing python function extend_recipe_sysroot
    NOTE: Direct dependencies are ['/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-core/glibc/cross-localedef-native_2.39.bb:do_populate_sysroot', '/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-core/glibc/ldconfig-native_2.12.1.bb:do_populate_sysroot', '/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/binutils/binutils-cross_2.42.bb:do_populate_sysroot', '/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/cdrtools/cdrtools-native_3.01.bb:do_populate_sysroot', '/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/qemu/qemuwrapper-cross_1.0.bb:do_populate_sysroot', '/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-kernel/kmod/depmodwrapper-cross_1.0.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-core/update-rc.d/update-rc.d_0.8.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/btrfs-tools/btrfs-tools_6.7.1.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/dosfstools/dosfstools_4.2.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/e2fsprogs/e2fsprogs_1.47.0.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/erofs-utils/erofs-utils_1.7.1.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/fdisk/gptfdisk_1.0.9.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/makedevs/makedevs_1.0.1.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/mtools/mtools_4.0.43.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/opkg-utils/opkg-utils_0.6.3.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/opkg/opkg_0.6.3.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/pseudo/pseudo_git.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/squashfs-tools/squashfs-tools_git.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/syslinux/syslinux_6.04-pre2.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-extended/parted/parted_3.6.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-extended/pigz/pigz_2.8.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-extended/xz/xz_5.4.7.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-support/bmaptool/bmaptool_git.bb:do_populate_sysroot']
    NOTE: Installed into sysroot: ['readline-native', 'dosfstools-native', 'gptfdisk-native', 'parted-native', 'popt-native']
    NOTE: Skipping as already exists in sysroot: ['base-files', 'base-passwd', 'gettext-minimal-native', 'cross-localedef-native', 'glibc', 'ldconfig-native', 'libxcrypt', 'systemd-systemctl-native', 'binutils-cross-aarch64', 'cdrtools-native', 'cmake-native', 'gcc-runtime', 'libgcc', 'libtool-native', 'm4-native', 'opkg-utils', 'qemu-native', 'qemuwrapper-cross', 'libpam', 'shadow-sysroot', 'shadow', 'texinfo-dummy-native', 'depmodwrapper-cross', 'linux-libc-headers', 'attr', 'ptest-runner', 'openssl-native', 'coreutils-native', 'dbus-native', 'expat-native', 'gettext-native', 'glib-2.0-native', 'libxml2-native', 'ncurses-native', 'update-rc.d-native', 'util-linux-libuuid-native', 'util-linux-native', 'zlib-native', 'btrfs-tools-native', 'desktop-file-utils-native', 'e2fsprogs-native', 'erofs-utils-native', 'flex-native', 'gnu-config-native', 'libedit-native', 'make-native', 'makedevs-native', 'mtools-native', 'nasm-native', 'opkg-utils-native', 'opkg-native', 'perl-native', 'pseudo-native', 'python3-build-native', 'python3-flit-core-native', 'python3-installer-native', 'python3-packaging-native', 'python3-pyproject-hooks-native', 'python3-setuptools-native', 'python3-six-native', 'python3-wheel-native', 'python3-native', 'squashfs-tools-native', 'syslinux-native', 'bzip2-native', 'groff-native', 'libarchive-native', 'libnsl2-native', 'libsolv-native', 'libtirpc-native', 'pigz-native', 'shadow-native', 'unzip-native', 'xz-native', 'zstd-native', 'gdk-pixbuf-native', 'gobject-introspection-native', 'gtk+3-native', 'cairo-native', 'fontconfig-native', 'freetype-native', 'harfbuzz-native', 'libjpeg-turbo-native', 'pango-native', 'libpthread-stubs-native', 'libx11-native', 'libxau-native', 'libxcb-native', 'libxcomposite-native', 'libxcursor-native', 'libxdamage-native', 'libxdmcp-native', 'libxext-native', 'libxfixes-native', 'libxft-native', 'libxi-native', 'libxrandr-native', 'libxrender-native', 'libxtst-native', 'pixman-native', 'xtrans-native', 'xcb-proto-native', 'xorgproto-native', 'util-macros-native', 'kmod-native', 'libpng-native', 'at-spi2-core-native', 'acl-native', 'attr-native', 'bmaptool-native', 'debianutils-native', 'fribidi-native', 'gdbm-native', 'icu-native', 'libbsd-native', 'libcap-ng-native', 'libffi-native', 'libmd-native', 'libpcre2-native', 'lz4-native', 'lzo-native', 'shared-mime-info-native', 'sqlite3-native']
    DEBUG: Python function extend_recipe_sysroot finished
    DEBUG: Executing python function set_image_size
    DEBUG: 8569485.600000 = 6591912 * 1.300000
    DEBUG: 8569485.600000 = max(8569485.600000, 65536)[8569485.600000] + 0
    DEBUG: 8569486.000000 = int(8569485.600000)
    DEBUG: 8569486 = aligned(8569486)
    DEBUG: returning 8569486
    DEBUG: Python function set_image_size finished
    DEBUG: Executing shell function do_image_wic
    INFO: Creating image(s)...

    ERROR: _exec_cmd: install -m 0644 /home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/Image /home/vysakh2/MNMI_SVSC/tisdk/build/arago-tmp-default-glibc/work/am62axx_evm-oe-linux/tisdk-default-image/1.0/tmp-wic/hdd/boot/Image returned '1' instead of 0
    output: install: cannot stat '/home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/Image': No such file or directory

    WARNING: /home/vysakh2/MNMI_SVSC/tisdk/build/arago-tmp-default-glibc/work/am62axx_evm-oe-linux/tisdk-default-image/1.0/temp/run.do_image_wic.629370:161 exit 1 from 'BUILDDIR="/home/vysakh2/MNMI_SVSC/tisdk/build" PSEUDO_UNLOAD=1 wic create "$wks" --vars "/home/vysakh2/MNMI_SVSC/tisdk/build/arago-tmp-default-glibc/sysroots/am62axx-evm/imgdata/" -e "tisdk-default-image" -o "$build_wic/" -w "$tmp_wic"'
    WARNING: Backtrace (BB generated script):
    #1: do_image_wic, /home/vysakh2/MNMI_SVSC/tisdk/build/arago-tmp-default-glibc/work/am62axx_evm-oe-linux/tisdk-default-image/1.0/temp/run.do_image_wic.629370, line 161
    #2: main, /home/vysakh2/MNMI_SVSC/tisdk/build/arago-tmp-default-glibc/work/am62axx_evm-oe-linux/tisdk-default-image/1.0/temp/run.do_image_wic.629370, line 197
    vysakh2@new:~/MNMI_SVSC/tisdk/build$

  • Hi,

    ERROR: _exec_cmd: install -m 0644 /home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/Image /home/vysakh2/MNMI_SVSC/tisdk/build/arago-tmp-default-glibc/work/am62axx_evm-oe-linux/tisdk-default-image/1.0/tmp-wic/hdd/boot/Image returned '1' instead of 0
    output: install: cannot stat '/home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/Image': No such file or directory

    wic can't find the kernel Image file because it's simply not in the deploy directory.

    Please run

    bitbake -e virtual/kernel | grep ^PN=
    bitbake -c deploy -f virtual/kernel

    If you are still getting errors, run the following.

    rm -f build/arago-tmp-default-glibc/stamps/am62axx_evm-oe-linux/*/*.do_deploy*
    bitbake tisdk-default-image

    Regards,
    Vinu

  • Hi Vinuchandran,

    Sorry for the late reply.

    After trying the both cases build showing this error.

    I will share the log

    tail -50 /home/vysakh2/MNMI_SVSC/tisdk/build/arago-tmp-default-glibc/work/am62axx_evm-oe-linux/tisdk-default-image/1.0/temp/log.do_image_wic.2350255
    DEBUG: Executing python function extend_recipe_sysroot
    NOTE: Direct dependencies are ['/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-core/glibc/cross-localedef-native_2.39.bb:do_populate_sysroot', '/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-core/glibc/ldconfig-native_2.12.1.bb:do_populate_sysroot', '/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/binutils/binutils-cross_2.42.bb:do_populate_sysroot', '/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/cdrtools/cdrtools-native_3.01.bb:do_populate_sysroot', '/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/qemu/qemuwrapper-cross_1.0.bb:do_populate_sysroot', '/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-kernel/kmod/depmodwrapper-cross_1.0.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-core/update-rc.d/update-rc.d_0.8.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/btrfs-tools/btrfs-tools_6.7.1.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/dosfstools/dosfstools_4.2.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/e2fsprogs/e2fsprogs_1.47.0.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/erofs-utils/erofs-utils_1.7.1.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/fdisk/gptfdisk_1.0.9.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/makedevs/makedevs_1.0.1.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/mtools/mtools_4.0.43.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/opkg-utils/opkg-utils_0.6.3.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/opkg/opkg_0.6.3.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/pseudo/pseudo_git.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/squashfs-tools/squashfs-tools_git.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-devtools/syslinux/syslinux_6.04-pre2.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-extended/parted/parted_3.6.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-extended/pigz/pigz_2.8.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-extended/xz/xz_5.4.7.bb:do_populate_sysroot', 'virtual:native:/home/vysakh2/MNMI_SVSC/tisdk/sources/oe-core/meta/recipes-support/bmaptool/bmaptool_git.bb:do_populate_sysroot']
    NOTE: Installed into sysroot: []
    NOTE: Skipping as already exists in sysroot: ['base-files', 'base-passwd', 'gettext-minimal-native', 'cross-localedef-native', 'glibc', 'ldconfig-native', 'libxcrypt', 'systemd-systemctl-native', 'binutils-cross-aarch64', 'cdrtools-native', 'cmake-native', 'gcc-runtime', 'libgcc', 'libtool-native', 'm4-native', 'opkg-utils', 'qemu-native', 'qemuwrapper-cross', 'libpam', 'shadow-sysroot', 'shadow', 'texinfo-dummy-native', 'depmodwrapper-cross', 'linux-libc-headers', 'attr', 'ptest-runner', 'openssl-native', 'coreutils-native', 'dbus-native', 'expat-native', 'gettext-native', 'glib-2.0-native', 'libxml2-native', 'ncurses-native', 'readline-native', 'update-rc.d-native', 'util-linux-libuuid-native', 'util-linux-native', 'zlib-native', 'btrfs-tools-native', 'desktop-file-utils-native', 'dosfstools-native', 'e2fsprogs-native', 'erofs-utils-native', 'gptfdisk-native', 'flex-native', 'gnu-config-native', 'libedit-native', 'make-native', 'makedevs-native', 'mtools-native', 'nasm-native', 'opkg-utils-native', 'opkg-native', 'perl-native', 'pseudo-native', 'python3-build-native', 'python3-flit-core-native', 'python3-installer-native', 'python3-packaging-native', 'python3-pyproject-hooks-native', 'python3-setuptools-native', 'python3-six-native', 'python3-wheel-native', 'python3-native', 'squashfs-tools-native', 'syslinux-native', 'bzip2-native', 'groff-native', 'libarchive-native', 'libnsl2-native', 'libsolv-native', 'libtirpc-native', 'parted-native', 'pigz-native', 'shadow-native', 'unzip-native', 'xz-native', 'zstd-native', 'gdk-pixbuf-native', 'gobject-introspection-native', 'gtk+3-native', 'cairo-native', 'fontconfig-native', 'freetype-native', 'harfbuzz-native', 'libjpeg-turbo-native', 'pango-native', 'libpthread-stubs-native', 'libx11-native', 'libxau-native', 'libxcb-native', 'libxcomposite-native', 'libxcursor-native', 'libxdamage-native', 'libxdmcp-native', 'libxext-native', 'libxfixes-native', 'libxft-native', 'libxi-native', 'libxrandr-native', 'libxrender-native', 'libxtst-native', 'pixman-native', 'xtrans-native', 'xcb-proto-native', 'xorgproto-native', 'util-macros-native', 'kmod-native', 'libpng-native', 'at-spi2-core-native', 'acl-native', 'attr-native', 'bmaptool-native', 'debianutils-native', 'fribidi-native', 'gdbm-native', 'icu-native', 'libbsd-native', 'libcap-ng-native', 'libffi-native', 'libmd-native', 'libpcre2-native', 'lz4-native', 'lzo-native', 'popt-native', 'shared-mime-info-native', 'sqlite3-native']
    DEBUG: Python function extend_recipe_sysroot finished
    DEBUG: Executing python function set_image_size
    DEBUG: 8569485.600000 = 6591912 * 1.300000
    DEBUG: 8569485.600000 = max(8569485.600000, 65536)[8569485.600000] + 0
    DEBUG: 8569486.000000 = int(8569485.600000)
    DEBUG: 8569486 = aligned(8569486)
    DEBUG: returning 8569486
    DEBUG: Python function set_image_size finished
    DEBUG: Executing shell function do_image_wic
    INFO: Creating image(s)...

    ERROR: _exec_cmd: install -m 0644 -D /home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/tiboot3.bin /home/vysakh2/MNMI_SVSC/tisdk/build/arago-tmp-default-glibc/work/am62axx_evm-oe-linux/tisdk-default-image/1.0/tmp-wic/hdd/boot/tiboot3.bin returned '1' instead of 0
    output: install: cannot stat '/home/vysakh2/MNMI_SVSC/tisdk/build/deploy-ti/images/am62axx-evm/tiboot3.bin': No such file or directory

    WARNING: /home/vysakh2/MNMI_SVSC/tisdk/build/arago-tmp-default-glibc/work/am62axx_evm-oe-linux/tisdk-default-image/1.0/temp/run.do_image_wic.2350255:161 exit 1 from 'BUILDDIR="/home/vysakh2/MNMI_SVSC/tisdk/build" PSEUDO_UNLOAD=1 wic create "$wks" --vars "/home/vysakh2/MNMI_SVSC/tisdk/build/arago-tmp-default-glibc/sysroots/am62axx-evm/imgdata/" -e "tisdk-default-image" -o "$build_wic/" -w "$tmp_wic"'
    WARNING: Backtrace (BB generated script):
    #1: do_image_wic, /home/vysakh2/MNMI_SVSC/tisdk/build/arago-tmp-default-glibc/work/am62axx_evm-oe-linux/tisdk-default-image/1.0/temp/run.do_image_wic.2350255, line 161
    #2: main, /home/vysakh2/MNMI_SVSC/tisdk/build/arago-tmp-default-glibc/work/am62axx_evm-oe-linux/tisdk-default-image/1.0/temp/run.do_image_wic.2350255, line 197
    vysakh2@new:~/MNMI_SVSC/tisdk/build$

  • Hi,

    This is the same failure signature, different file.

    Now tiboot3.bin (the R5 SPL/bootloader stage) is missing for the exact same reason (No such file or directory, stamp says done, file isn't there).

    Resolving recipe-by-recipe with -f deploy each time you hit a new missing file will be tedious.

    With the earlier command, the a53 side got cleared, but the r5 core stamps remain.

    Do the following to find all the stamps from build directory and delete them.

    find build -path '*/stamps/*' -name '*.do_deploy*' -delete
    bitbake tisdk-default-image

    Regards,
    Vinu

  • Hi Vinuchandran,

    This resloved my issue. 
    Thanks for the support.