AM62A7: Test utility to increase the CPU and DSP load to increase power consumption

Part Number: AM62A7

Hi, 

We are performing the stress testing on our device which is based on the AM62A7 processor. Our aim is to provide the stress on the CPU and DSP and increase the power consumption on the AM62A7 processor.

We have tried to use the "vx_app_load_test.out" to provide load on the C7x. 

/opt/vision_apps/vx_app_load_test.out 2 80 60

Above command will provide the 80% load on the C7x. But this utility doesn't excersize the MMA (matrix multiply accelerator) and only loads the scalar/vector of C7x pipeline. If MMA of C7x is used then only it consumes more power. 

So, there any other utilty for C7x to which can provide load on MMA and increase power consumption?

Providing the load on the CPU doesn't increase the power consumption. So, Is there any other utility available to excersize the power consumption of the board?

Regards,
Jay