AM623: AM62X BCDMA TRPD Flags Questions

Part Number: AM623

Hello,

I have a question about the different BCDMA TRPD flags. In SPRUIV7B Table 11-42 I see the STATIC bit declared in bit 4 of the FLAGS field, but in Table 11-43 bit 4 is set to Reserved. Additionally I see the MCU+SDK and the TI PSDK for QNX define the CMD_ID field starting at bit 16 but both Table 11-42 and Table 11-43 in the TRM decribe that as Reserved as well. Could you confirm if the STATIC and CMD_ID flags are implemented by the AM62x family or if these flags were simply inherited by the AM64x or AM65x as part of a common structure for all TI SoCs?

In the TRM bits 24-31 are described as Configuration Specific Flags. In the MCU+SDK and TI PSDK these are defined as source and destination indirection flags, SUPR_EVT, EOL, and EOP flags. Can you confirm that these flags are also used by the AM62x family of SoC?

Thanks for your help!

From,

Daniel Fettke