Part Number: AM3352
Hi,
This is the question related with the thread as follows.
According to the thread above, RTC scratch register can be used to store data before warm reset and keep it after warm reset.
Howver, customer wants to save more data. So they try to use alarm register. Here is question.
- In the ALARMSEC0 field (4-bits) of ALARM_SECONDS_REG register, TRM says user should set 0 to 9. However, customer wants to use whole 4-bits (0 to 15). Is it ok? Even if we cannot officially allow them to do, can we say technically ok at their risk. They do not start RTC counter.
- Is there any potential risk to use ALARM_SECONDS_REG register to save data? Again, customer does not start RTC. For me, it looks there is no risk.
Thank you.
Best Regards,
Kasai