J722SXH01EVM: Guidance required for IMX728 camera bring-up on J722SXH01EVM with Linux SDK

Part Number: J722SXH01EVM
Other Parts Discussed in Thread: J7EXPA01EVM

Hi TI-Team, 

. From the TI Imaging release notes, I found the following D3 Embedded page for Sony IMX728 cameras with FPD-Link IV interface: https://www.d3embedded.com/product-category/camera-modules/?fwp_platform=texas-instruments&fwp_interface=fpd-link-iv&fwp_sensor_model=sony-imx728-

 

Could you please confirm whether this is the correct camera family for use with the J722SXH01EVM and the IMX728 setup supported by TI?

 

I also wanted to ask about one more possibility before we purchase a new camera.

 

Our current camera is:

LI-IMX728RCCB-96717-120H-DSL
Serializer: MAX96717
Interface: GMSL2

 

We understand from your previous reply that GMSL2 and TI FPD-Link are not directly compatible.

 

Since the J722SXH01EVM provides MIPI CSI-2 inputs through J36/J37, would it be technically possible to use our existing MAX96717-based GMSL2 IMX728 camera with an external GMSL2 deserializer that outputs MIPI CSI-2 to J36/J37?

 

We understand that this would bypass TI’s FPD-Link/Fusion deserializer. Could you please advise whether TI has any known or recommended approach for such a setup, and what software changes would be required in the device tree, deserializer driver and IMX728 camera integration?

 

If using the existing GMSL2 camera is not practical or not supported, then we will proceed with the TI-supported FPD-Link IV IMX728 camera.

 

Thank you for your guidance!

Best regards,

Jens