This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Issue with Opening USB port on BeagleBoard-xm running Gingerbread pre-built image



I'm new to beagleboard and running gingerbread pre-built image. I need to create new rule under udev for allowing some USB devices to be able to open the port. Also, I need to make change to init.rc so that this solution is permanent. Can somebody help me since neither I could find udev nor init.rc this pre-built image?   - kjs