Hi all,
I am trying to compie a minimum arago image following this page :
http://arago-project.org/wiki/index.php/Setting_Up_Build_Environment
When I launch the command
Hi all,
I am trying to compie a minimum arago image following this page :
http://arago-project.org/wiki/index.php/Setting_Up_Build_Environment
When I launch the command bitbake arago-base-image it fails like this :
Connexion vers sources.openembedded.org|140.211.169.152|:80...NOTE: fetch http://sources.openembedded.org//git_git.savannah.gnu.org.config.git_e35217687ee5f39b428119fe31c7e954f6de64f0.tar.gz
connecté.
requête HTTP transmise, en attente de la réponse...NOTE: package perl-native-5.10.1-r10: task do_patch: Succeeded
404 Not Found
2012-02-23 17:26:42 ERREUR 404: Not Found.
--2012-02-23 17:26:43-- http://arago-project.org/files/sources/git_git.savannah.gnu.org.config.git_e35217687ee5f39b428119fe31c7e954f6de64f0.tar.gz
Résolution de arago-project.org... 184.73.161.183
Connexion vers arago-project.org|184.73.161.183|:80...connecté.
requête HTTP transmise, en attente de la réponse...NOTE: Running task 25 of 3832 (ID: 571, virtual:native:/home/jm/work/vodabox/sources/arago-gstti/arago-oe-dev/recipes/unifdef/unifdef_2.6.bb, do_qa_configure)
NOTE: package unifdef-native-2.6-0: task do_qa_configure: Started
NOTE: package unifdef-native-2.6-0: task do_qa_configure: Succeeded
404 Not Found
2012-02-23 17:26:43 ERREUR 404: Not Found.
ERROR: TaskFailed event exception, aborting
ERROR: Build of virtual:native:/home/jm/work/vodabox/sources/arago-gstti/arago-oe-dev/recipes/gnu-config/gnu-config_git.bb do_fetch failed
NOTE: Running task 26 of 3832 (ID: 572, virtual:native:/home/jm/work/vodabox/sources/arago-gstti/arago-oe-dev/recipes/unifdef/unifdef_2.6.bb, do_compile)
NOTE: fetch http://arago-project.org/files/sources/git_git.savannah.gnu.org.config.git_e35217687ee5f39b428119fe31c7e954f6de64f0.tar.gz
ERROR: Task 372 (virtual:native:/home/jm/work/vodabox/sources/arago-gstti/arago-oe-dev/recipes/gnu-config/gnu-config_git.bb, do_fetch) failed with exit code 1
NOTE: package unifdef-native-2.6-0: task do_compile: Started
NOTE: Task failed: Fetch failed: Unable to fetch URL http://www.angstrom-distribution.org/unstable/sources/git_git.savannah.gnu.org.config.git_e35217687ee5f39b428119fe31c7e954f6de64f0.tar.gz from any source.
NOTE: package gnu-config-native-git-r1+gitre35217687ee5f39b428119fe31c7e954f6de64f0-arago1: task do_fetch: Failed
ERROR: TaskFailed event exception, aborting
NOTE: package quilt-native-0.48-r7.1: task do_install: Succeeded
ERROR: Build of virtual:native:/home/jm/work/vodabox/sources/arago-gstti/arago-oe-dev/recipes/gnu-config/gnu-config_git.bb do_fetch failed
ERROR: Task 372 (virtual:native:/home/jm/work/vodabox/sources/arago-gstti/arago-oe-dev/recipes/gnu-config/gnu-config_git.bb, do_fetch) failed with exit code 1
Waiting for 2 active tasks to finish:
1: unifdef-native-2.6-0 do_compile (pid 29668)
2: linux-libc-headers-native-2.6.31-r6 do_unpack (pid 28967)
Waiting for 1 active tasks to finish:
1: linux-libc-headers-native-2.6.31-r6 do_unpack (pid 28967)
NOTE: package unifdef-native-2.6-0: task do_compile: Succeeded
ERROR: 'virtual:native:/home/jm/work/vodabox/sources/arago-gstti/arago-oe-dev/recipes/gnu-config/gnu-config_git.bb' failed
NOTE: package linux-libc-headers-native-2.6.31-r6: task do_unpack: Succeeded
ERROR: 'virtual:native:/home/jm/work/vodabox/sources/arago-gstti/arago-oe-dev/recipes/gnu-config/gnu-config_git.bb' failed
ERROR: 'virtual:native:/home/jm/work/vodabox/sources/arago-gstti/arago-oe-dev/recipes/gnu-config/gnu-config_git.bb' failed
I understand that it tries to download the file from http://arago-project.org/files/sources/git_git.savannah.gnu.org.config.git_e35217687ee5f39b428119fe31c7e954f6de64f0.tar.gz and fails but why is it looking for this one ?
How can I solve this issue ?
Thanks in advance,
Regards,
JM