Part Number: SK-AM62A-LP
Other Parts Discussed in Thread: AM62A3, AM62A7
Hello,
I encountered some problems booting on SD card on my own board (similar to the SK-AM62A-LP) with a dual-core AM62A3.
The .wic file was made from SDK 11.01.05.07 with Yocto and the only file modified was the k3-am62a7.dtsi by deleting the lines related to two of the four CPUs. This file is properly working with the same board but with a quad-core AM62A7. However, with the dual-core AM62A3, it does not work at all (not even a single character in the console during boot).
Is deleting these lines sufficient to work, or do I need to modify other things for the AM62A32 ?