Hi all;
Nand (512MB) is at chip select 0! => Working fine!!!!!!!!!!!!
Now i need to access the nand at chip select 7!
I modifiied set of files in AM3703 Board!
NCS7 ==> Base Address = 0x38000000 !!!!!!!!! IF IT IS WRONG PLZ SUGGEST CORRECT ADDRESS?
PIN_MUX = (NCS7) = (MUX_VAL(CP(GPMC_NCS7), (IDIS | PTU | EN | M0)) /*GPMC_NCS7*/\ ==> beagle.h
mem.h ==> All gpmc registers are set ! ==> GPMC_CONFIG1-7 registers!
mem.c ==> Enabling the CS7!
NAND PART NUMBER = Micron => MT29F16G08ABABA!!!!!!!!!!!
Need help????????????
Regards,
santosh vastrad