Hi,
I am trying to build the application after booting the board with the uimage built and mounting the filesystem using nfs.
I am getting the following bootlog but after that it hangs:
DM368 IPNC :>
DM36x initialization passed!
TI UBL Base Version: 1.50
Boot Loader BootMode = NAND
Starting NAND Copy...
Valid magicnum, 0xA1ACED66, found in block 0x00000008.
Boot Mode Task Completed
IPNC UBL Version: 1.1.0
Platform: DM368
Jumping to entry point at 0x81080000
U-Boot 1.3.4 (Dec 9 2010 - 17:44:14) DM368-IPNC-1.0.1
I2C: ready
DRAM: 128 MB
NAND: NAND device: Manufacturer ID: 0xec, Chip ID: 0xf1 (Samsung NAND 128MiB 3,3V 8-bit)
Bad block table found at page 65472, version 0x01
Bad block table found at page 65408, version 0x01
128 MiB
In: serial
Out: serial
Err: serial
ARM Clock :- 432MHz
DDR Clock :- 340MHz
Ethernet PHY: GENERIC @ 0x01
Hit any key to stop autoboot: 0
Loading from NAND 128MiB 3,3V 8-bit, offset 0x500000
Image Name: Linux-2.6.18_pro500-davinci_IPNC
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1883716 Bytes = 1.8 MB
Load Address: 80008000
Entry Point: 80008000
## Booting kernel from Legacy Image at 80700000 ...
Image Name: Linux-2.6.18_pro500-davinci_IPNC
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 1883716 Bytes = 1.8 MB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Linux version 2.6.18_pro500-davinci_IPNC_DM368_2.6.0 (root@mayank-a) (gcc version 4.2.0 (MontaVista 4.2.0-16.0.32.0801914 2008-08-30)) #1 PREEMPT Fri Feb 24 11:52:18 I2
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
Machine: DaVinci DM368 IPNC
Memory policy: ECC disabled, Data cache writeback
DaVinci DM0365 variant 0x8
PLL0: fixedrate: 24000000, commonrate: 170000000, vpssrate: 340000000
PLL0: vencrate_sd: 75555555, ddrrate: 340000000 mmcsdrate: 48571428
PLL1: armrate: 432000000, voicerate: 20571428, vencrate_hd: 27000000
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
Built 1 zonelists. Total pages: 14336
Kernel command line: console=ttyS1,115200n8 noinitrd rw ip=192.168.1.10:192.168.1.50:255.255.255.0 root=/dev/nfs nfsroot=192.168.1.50:/home/mayank/DM368Aptina/ipnc/tarM
PID hash table entries: 256 (order: 8, 1024 bytes)
Clock event device timer0_0 configured with caps set: 07
Console: colour dummy device 80x30
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory: 56MB = 56MB total
Memory: 52608KB available (3229K code, 658K data, 184K init)
Security Framework v1.0.0 initialized
Capability LSM initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
NET: Registered protocol family 16
DaVinci: 104 gpio irqs
MUX: initialized GPIO20
MUX: initialized I2C_SCL
Generic PHY: Registered new driver
ch0 default output "COMPOSITE", mode "NTSC"
VPBE Encoder Initialized
SCSI subsystem initialized
NET: Registered protocol family 2
IP route cache hash table entries: 512 (order: -1, 2048 bytes)
TCP established hash table entries: 2048 (order: 1, 8192 bytes)
TCP bind hash table entries: 1024 (order: 0, 4096 bytes)
TCP: Hash tables configured (established 2048 bind 1024)
TCP reno registered
VFS: Disk quotas dquot_6.5.1
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
squashfs: version 3.1 (2006/08/19) Phillip Lougher
JFFS2 version 2.2. (NAND) (C) 2001-2006 Red Hat, Inc.
yaffs Feb 24 2012 11:50:27 Installing.
SGI XFS with no debug enabled
Initializing Cryptographic API
io scheduler noop registered
io scheduler anticipatory registered (default)
LTT : ltt-facilities init
LTT : ltt-facility-core init in kernel
DAVINCI-WDT: DaVinci Watchdog Timer: heartbeat 60 sec
Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO map 0x1c20000 mem 0xfbc20000 (irq = 40) is a 16550A
serial8250.0: ttyS1 at MMIO map 0x1d06000 mem 0xfbd06000 (irq = 41) is a 16550A
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize
Davinci EMAC MII Bus: probed
MAC address is deadbeaf
TI DaVinci EMAC Linux version updated 4.0
netconsole: not configured, aborting
Linux video capture interface: v2.00
Trying to register davinci display video device.
layer=c067b000,layer->video_dev=c067b160
Trying to register davinci display video device.
layer=c0655e00,layer->video_dev=c0655f60
davinci_init:DaVinci V4L2 Display Driver V1.0 loaded
i2c /dev entries driver
Generic platform RAM MTD, (c) 2004 Simtec Electronics
nand_davinci nand_davinci.0: Using 4-bit hardware ECC
NAND device: Manufacturer ID: 0xec, Chip ID: 0xf1 (Samsung NAND 128MiB 3,3V 8-bit)
Creating 6 MTD partitions on "nand_davinci.0":
0x00000000-0x00300000 : "bootloader"
mtd: Giving out device 0 to bootloader
0x00300000-0x00500000 : "params"
mtd: Giving out device 1 to params
0x00500000-0x00700000 : "kernel"
mtd: Giving out device 2 to kernel
0x00700000-0x01f00000 : "filesystem"
mtd: Giving out device 3 to filesystem
0x01f00000-0x02100000 : "data1"
mtd: Giving out device 4 to data1
0x02100000-0x08000000 : "data2"
mtd: Giving out device 5 to data2
nand_davinci nand_davinci.0: hardware revision: 2.3
MUX: initialized SPI0_SCLK
MUX: initialized SPI0_SDO)
MUX: initialized SPI0_SDI
My bootargs is as follows:
bootdelay=4
baudrate=115200
bootfile="uImage"
setboot=setenv bootargs $(bootargs)
eth=00:01:02:03:04:05
bootcmd=nboot 0x80700000 0 0x500000;bootm 0x80700000
ethaddr=00:01:02:03:04:05
dnsip=192.168.1.1
dnsip2=192.168.1.1
bootargs=console=ttyS1,115200n8 noinitrd rw ip=192.168.1.10:192.168.1.50:255.255.255.0 root=/dev/nfs nfsroot=192.168.1.50:/home/mayank/DM368Aptina/ipnc/target/filesys,M
filesize=1CBE84
fileaddr=80700000
gatewayip=192.168.1.1
netmask=255.255.255.0
ipaddr=192.168.1.10
serverip=192.168.1.50
stdin=serial
stdout=serial
stderr=serial
ver=U-Boot 1.3.4 (Dec 9 2010 - 17:44:14) DM368-IPNC-1.0.1
Environment size: 622/131068 byte
.
I am not able to get why it hangs in between
Thanks and Regards,
Mayank