This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3517 Problem with kernel (booting)

Hello!

 

I use the x-loader, u-boot and the kernel from the cd of variscite and when I want to boot, then the following errors appear:

...

Setting autofs.
Setup fonts.
Setting PowerVR consumer services.
omaplfb: Unknown symbol omap_dispc_unregister_isr
omaplfb: Unknown symbol omap_dispc_register_isr
modprobe: can't load module omaplfb (/lib/modules/2.6.32/kernel/drivers/char/oma
plfb.ko): unknown symbol in module, or unknown parameter
Failed to load omaplfb
Exec QtDemo.
starting pid 571, tty '': '/sbin/getty -L ttyS2 115200 vt100 '
PHY: ffffffff:00 - Link is Up - 100/Full

(none) login: /dev/fb0: No such file or directory
Could not initialize EGL display - are the drivers loaded?
/dev/fb0: No such file or directory
powervr: driver cannot connect

 

The settings of the fb are:

 

#
# Graphics support
#
# CONFIG_VGASTATE is not set
# CONFIG_VIDEO_OUTPUT_CONTROL is not set
CONFIG_FB=y
# CONFIG_FIRMWARE_EDID is not set
# CONFIG_FB_DDC is not set
# CONFIG_FB_BOOT_VESA_SUPPORT is not set
CONFIG_FB_CFB_FILLRECT=y
CONFIG_FB_CFB_COPYAREA=y
CONFIG_FB_CFB_IMAGEBLIT=y
# CONFIG_FB_CFB_REV_PIXELS_IN_BYTE is not set
# CONFIG_FB_SYS_FILLRECT is not set
# CONFIG_FB_SYS_COPYAREA is not set
# CONFIG_FB_SYS_IMAGEBLIT is not set
# CONFIG_FB_FOREIGN_ENDIAN is not set
# CONFIG_FB_SYS_FOPS is not set
# CONFIG_FB_SVGALIB is not set
# CONFIG_FB_MACMODES is not set
# CONFIG_FB_BACKLIGHT is not set
# CONFIG_FB_MODE_HELPERS is not set
# CONFIG_FB_TILEBLITTING is not set

#
# Frame buffer hardware drivers
#
# CONFIG_FB_S1D13XXX is not set
# CONFIG_FB_VIRTUAL is not set
# CONFIG_FB_METRONOME is not set
# CONFIG_FB_MB862XX is not set
# CONFIG_FB_BROADSHEET is not set
# CONFIG_FB_OMAP_BOOTLOADER_INIT is not set
CONFIG_OMAP2_VRAM=y
CONFIG_OMAP2_VRFB=y
CONFIG_OMAP2_DSS=y
CONFIG_OMAP2_VRAM_SIZE=4
# CONFIG_OMAP2_DSS_DEBUG_SUPPORT is not set
# CONFIG_OMAP2_DSS_RFBI is not set
CONFIG_OMAP2_DSS_VENC=y
CONFIG_OMAP2_VENC_OUT_TYPE_SVIDEO=y
# CONFIG_OMAP2_VENC_OUT_TYPE_COMPOSITE is not set
# CONFIG_OMAP2_DSS_SDI is not set
CONFIG_OMAP2_DSS_DSI=y
CONFIG_OMAP2_DSS_USE_DSI_PLL=y
# CONFIG_OMAP2_DSS_FAKE_VSYNC is not set
CONFIG_OMAP2_DSS_MIN_FCK_PER_PCK=1
CONFIG_FB_OMAP2=y
# CONFIG_FB_OMAP2_DEBUG_SUPPORT is not set
# CONFIG_FB_OMAP2_FORCE_AUTO_UPDATE is not set
CONFIG_FB_OMAP2_NUM_FBS=1

I don't need the video part and touchscreens and so on, but even if I want to disable them, then I get the errors.

Does anyone of you please could help me? I'm a newbie and don't have that much experience.

 

Thanks in advance!