Part Number: AM62A7
We want to use the wkup serial port exclusively under Linux (A53). Therefore, we want the device manager (DMR5) to stop using this serial connection; to do this, we are using the board configuration information from the tiboot3.bin file.
Currently, we still see “##DM Built On: ...” on the wkup serial port, even though the tiboot3-am62ax-hs-evm.bin file was built using board-cfg.bin and combined-dm-cfg.bin. The board-cfg.bin file was built from board-cfg.yaml with “trace_dst_enables: 0x00”.
Does the version tagged “11.01.07” of the dm_edgeai_mcu1_0_release_strip.out firmware in processor-firmware/ti-linux-firmware.git actually use the trace_dst_enables field?
other UART using syconfig tool in MCU_PLUS_SDK. rebuild DM firmware.