This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3715 maximum consumption

Other Parts Discussed in Thread: AM3715

I'm in the process of sizing the power supplies for an AM3715 application. I used the power estimation spreadsheet to estimate the max current the processor would draw from its various rails for our use case (attached). The following assumptions were made: max temp 50C, max operating freq would be OPP100 (600 MHz), and all peripherals would be used with the exception of MMC 2, 3 and the DAC.

Would it be safe to size the supplies against the currents as reported in this spreadsheet? I plan to oversize by ~30%.

Thanks - AM

3438.Power Estimation AM37x v1_01.xls