This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Face Detection Demo- Problem in Importing project



I am unable to import the demo project( face detection) obtained after downloading c6sdk_1_00_00_03. The problem is-

Error  loading managed make project information for face detect. The tool definitions used to create the project are not available.

If I try to create a new project and add the files, the error is-

js: "D:/ccs4installed/xdctools_3_22_02_27/include/utils.tci", line 582: Error: Can't find import file: '../../../../pdk_C6748_1_0_0_1/packages/ti/pspiom/platforms/evmOMAPL138/vpif.tci' (not found along 'D:\ccs4installed\workspace\trial2\Release/../;D:/ccs4installed/bios_5_41_10_36/packages;;D:\ccs4installed\xdctools_3_22_02_27/include;D:\ccs4installed\xdctools_3_22_02_27/packages')
gmake: *** [facedetectcfg.cmd] Error 1

Please help

  • Please follow the instructions on the User Guide in section Building the software. If you follow the instructions you will be able to import the existing CCS project in CCSv4. Please check your CGTools installation and include the correct CGTools identified by the CCS. It is recommended to use CGTools 7.3. Add the paths for the environment variables in the project if they are different.

    Regards

    Asheesh