Other Parts Discussed in Thread: TPS65950, AM3715
Hi all
I have a Mistral AM37xx EVM that comes with a 26MHz clock and 256MB of LPDDR RAM. On a custom built board that is pretty much like the EVM, I will have a 13 MHz crystal instead of a 26MHz and I was wondering if that would affect the RAM. I found a function in xloader that apparently detects the frequency of the clock and sets a register with this value, but I cant be sure that RAM will work just fine. I did try to change the frequency on the Mistral EVM to see if RAM was affected, but I was not able to find a way to do so.
Anybody could help me with this?
Thanks
RS