Part Number: AM2754-Q1
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM2754-Q1
Hello,
the same table for HyperRAM does not exist, there is no mandatory locations where resources must be placed with a couple of exceptions that I will highlight here. It is also not possible to boot from HyperRam like you do from DDR, so SBL and app images are not expected in a specific location by ROM or SBL code, respectively.
The HyperRAM start address in the AM275x memory map is 0x6800_0000, called "FSS1_DAT_REG1" in the TRM:

The whole region can be configured as data memory, but the following regions must be defined in your project as to not extend into the memory mapped regions of the CR and ID registers of the hyperram memory:
General HyperRAM region definition:

ID registers region definition:

CR registers region definition:

Best,
Daniel