Other Parts Discussed in Thread: TMS320C6678
Hi all,
I learned from a earlier post that It is poossible to boot C6678 directly from SPI Nor Flash, without the participation of I2C. But another post holds the view that FPGA is
programmed to force the DSP boots from the I2C regardless of the boot strapping ,then it re-enters the bootrom and boots using the mode selected.This is due to the
PLL fix.
Now I am very confused with the following issues:
1. Can C6678 be booted up directly from SPI Nor Flash,without the participation of I2C ?
2.Is it necessary to program IBL and IBL configuration on I2C EEPROM at bus address 0x51 when I test SPI boot mode on TMDXEVM6678L Rev0.2 ?
Thanks in advance.
Nuoxi Lin.