Part Number: J784S4XEVM
Other Parts Discussed in Thread: J7EXPA01EVM
Hi TI Expert,
Using the J7EXPA01EVM board connected to the J784S4EVM board.
Testing with one IMX390 camera module connected to the J4 connector of the J7EXPA01EVM board.

If you run the launch.js file and load and run the following executable file on R5 MCU2_0 as follows, the following log is generated through the serial port.


-----------------------------------------------------------------------------------------------------------
FWL Bit 0x1C
Exception addr 0x45B0A000
FWL Exception 0x1127000
0x30000
0x32C57004
0x0
0xA8922D8
0x4
------------------------------------------------------------------------------------------------------------
I want to know what the problem is.