Hi,
I am using the USB CDC class from the Stellaris library (revision 6288 ) on C6748.
I am using the "usb_dev_serial_c674x_c6748_evmC6748" example without the UART side (I want to communicate with PC only, no actual RS232 or UART) and from the functional aspect everything is OK, I can send/receive buffers from/to PC/device.
I have an issue with the bit rate which is very slow: I am sending the 150 K[Byte] in about 1.1 [sec] .
I understood that events: USBD_CDC_EVENT_GET_LINE_CODING and USBD_CDC_EVENT_SET_LINE_CODING have nothing to do with the real USB bit rate (maybe I am wrong, I used thous and had no improvements or affect what so ever).
- How can I increase the bit rate to high/full USB bit rates?
- What maximum bit rate can I expect from this USB library class?