AM6422: XDP-Zero Copy on AM64

Part Number: AM6422

Dear Experts,
Znfortunately it seems like XDP Zero Copy  this is not working properly with our Application (EtherCat Master running over ICSSG)  with activated XDP Zero Copy.
FTrace/Kernel shows a behaviour that was not expected. 
It seems like  TX/Rx handling is moved towards ksoftirqd (softirqs NET_RX, NET_TX) and interrupted by ICSSG in between. The time to handle tx & rx seems to be significantly higher than expected.
 Regards,
Alex

  • Hello Alex,

    What version of software is being run?

    Regards,

    Nick

  • Hi Alex, Customer Team, 

    I ran a test this afternoon with the following setup 

    1. AM62Px - 4 slaves setup to control 8 axes

    2. Moved my EtherCAT RX and TX IRQs to CPU3 (same CPU core as EtherCAT_Task)

    3. Elevated my EtherCAT RX and TX IRQs to priority 57 to be higher than EtherCAT_Task (EtherCAT_Task priority was at 56) 

    4. NOTE: DID NOT YET try the "WaitForPacket" parameter since I wanted to start simple. I may test this next

    5. Captured kernel trace with this setup (trace-customer-090326) and compared with my previous configuration with RX and TX IRQs on CPU2 and at same priority as EtherCAT_Task (trace-090226). Please below zip files for the traces. 

    trace-customer-090326.zip

    trace-090226.zip

    trace-customer-090826.zip

    Below is list of my observations and theories to why might be occurring regarding the larger than expected ksoftirqd execution times:

    trace-260625-xdp_zero-copy-rx-delay-1325.dat

    Customer provided trace

    trace-customer-090326.dat

    TI emulating customer setup

    trace-customer-090826.dat

    TI emulating customer setup

    trace-090226.dat

    TI original setup

    ksoftirq execution time ~165us ~100us ~159us ~26us
    EtherCAT_Task interrupted by ksoftirq? Yes No No No
    ksoftirq events that show up

    irq_handler_entry for icssg1-eth-tx0 + other irq related events

    irq_handler_entry for ethernet-tx0 + other irq related events irq_handler_entry for ethernet-tx0 + other irq related events no irq_handler_entry or irq related events
    EtherCAT port TX and RX IRQ handling theories IRQs on CPU1 are competing for processing time with EtherCAT_Task which leads to ksoftirq irq related events being triggered 

    IRQs on CPU3 are competing for processing time with EtherCAT_Task which leads to ksoftirq irq related events being triggered 

    Next: need to test IRQs on CPU3 in isolation (from IRQs higher priority) to see if truly same CPU that cause the competition for resources or the higher priority that is the cause

    Tested IRQs on CPU3 in isolation from IRQs at higher priority from EtherCAT_Task and still see that ksoftirq with irq_handler_entry events appear → indicates that as long as on same CPU core, then will be competing with processing time with EtherCAT_Task

    ksoftirq execution time is also much larger than trace-customer-090326.dat when IRQs are same priority as EtherCAT_Task...

    IRQs moved to dedicated CPU2 where no ksoftirq events observed because no competing resources leading to needing ksoftirq to be triggered

    the ksoftirq events on CPU3 are not related to handling IRQs which is why shorter execution time

    Theories to EtherCAT_Task interruption
    1. WaitForPacket parameter
    2. IRQs higher in priority than EtherCAT_Task

    IRQs were higher in priority than EtherCAT_Task and while trace doesn't capture interruption of EtherCAT_Task, later on cycle time had spiked to ~1552us indicating likely EtherCAT_Task was interrupted by some event (could be IRQs)

    Next: try running with WaitForPacket parameter

    Only ran for ~15 minutes and during this time did not see cycle time spike 

    Next: try running with WaitForPacket parameter

    No interruption occurred

    From these results and comparison I think that the real solution to eliminating the irq handler events from ksoftirqd is to have a dedicated core to handle RX and TX IRQ processing of the EtherCAT port.

    I don't yet have the solution to EtherCAT_Task being interrupted will need to look into it further (could simply be because IRQs higher in priority than EtherCAT_Task).

    -Daolin

  • Update:

    I realized that some cycles from the trace-customer-090326.dat had larger ksoftirq execution time so I have corrected the execution time in the table above. With the correction, the execution time is ~100us closer to what was observed on trace-260625-xdp_zero-copy-rx-delay-1325.dat. 

    I've also added to the above table a test I did today with only setting IRQs to same CPU core as EtherCAT_Task but keeping the priority the same as EtherCAT_Task. It looks like its not increasing the IRQ priority that caused ksoftirq execution time but that the IRQs are on the same core as EtherCAT_Task.

    I'm working on testing with WaitForPacket parameter next. On initial test, I see that the RxErrorCount statistic from the IDE increment rapidly. Is this something you have also noticed on your setup when testing with the WaitForPacket parameter?

    -Daolin

  • Hello,

    In addition to the tests we discussed in the call for customer to try, can customer also try moving the Ethernet TX and RX IRQ to CPU0 instead of CPU1?

    From what I found about the "WaitForPacket" parameter, this parameter requires the EtherCAT frame to be received on the same cycle as when it was transmitted as opposed to being received on the next cycle. If there are ksoftirq events like irq_handler_entry events showing up, this will significantly increase ksoftirq execution time therefore also increasing the time EtherCAT_Task is interrupted. The goal is to move this to another CPU core that wouldn't have to share resources with EtherCAT_Task core. Since only CPU0 is available as the other core, you should give that a try as a sanity check. 

    I will try to investigate if the TX and RX IRQs can be handled by R5 core if the main application program (EtherCAT_Task is on A53 core), at this moment in time, I'm not sure if it is possible.

    -Daolin

  • We have managed to capture initial traces on the CPSW (using a mix: one interface via CPSW for EtherCAT and one via PRU-ETH for everything else). However, this was done without core isolation, pinning and interrupt prioritization — simply to see if the "ksoftirqd effect" is fundamentally present there as well. Surprisingly, neither ksoftirqd nor the interrupts (!) appeared in the traces in this instance — neither for the CPSW nor the PRU-ETH.
    We therefore intend to repeat the tests: This time with core isolation, pinning and interrupt prioritization, to confirm our observations under the same conditions as before. This is currently being prepared.

    We will also then check for pinning Ethernet TX and RX IRQs to the other core.

  • Hi Florian, 

    Thanks for the update on your next steps. 

    I will try to investigate if the TX and RX IRQs can be handled by R5 core if the main application program (EtherCAT_Task is on A53 core), at this moment in time, I'm not sure if it is possible.

    One question I have for you regarding this, do you have a specific requirement to only use A53 cores for EtherCAT or are receptive to mapping IRQs to R5 cores if it is possible?

    -Daolin

  • Hi Daolin,

    If that is possible, we could consider doing that

    To my knowledge up to now we're not using R5 at all. But if we wanted to do this in future, it would be interesting to know, if that then could co-exist with the IRQ handling (if possible at all)?

    The user logic executed as part of the EtherCAT cycle, at the moment definitely needs to be executed on A53, since CODESYS has no compiler backend for R5 and in general - to my knowledge - no concept for this kind of asymmetric multicore architecture.

    I'll share the traces as soon as we repeated the test.

    -Florian

  • Hi Florian, 

    Apologies for the delay in response. 

    To my knowledge up to now we're not using R5 at all. But if we wanted to do this in future, it would be interesting to know, if that then could co-exist with the IRQ handling (if possible at all)?

    Unfortunately after discussing internally about using the R5 core to handle IRQ processing, we don't think using the R5 cores while using A53 for CODESYS will be a viable solution. The reason is because our only current example of tunneling between the A53 and R5 will have too much latency, my understanding is >3ms which is definitely not fast enough to meet EtherCAT cycle times. 

    If I may ask, is there a hard requirement to use CODESYS for your application? Since you are trying to implement an EtherCAT use case on AM64x which has 4 R5 but only 2 A53, why not use an EtherCAT stack capable of running on R5 cores?

    Additionally, this week a colleague of mine was able to recreate the behavior you observed on an AM64x EVM with ICSSG port (the IDE port being CPSW) with XDP ZC and the WaitForPacket enabled. We also tried moving the TX and RX IRQs from CPU1 to CPU0 and found some potential improvements in EtherCAT_Task execution time compared to if the IRQs remained on CPU1. Unfortunately, there doesn't appear to be a solution to completely remove the EtherCAT_Task from being interrupted but I think that is to be expected with WaitForPacket, based on what I understand how WaitForPacket is supposed to work. 

    My colleague will share the results of our capture shortly on this thread.

    -Daolin

  • Hi, 

    Here are the results from our experiments with moving the IRQs from CPU1 to CPU0

    core_isolation.zip
    Preface:

    • CPU1 isolated with only EtherCAT_Task and select IRQs
    • CPU0 contains the other CODESYS child tasks and OS housekeeping tasks
    • XDP_ZeroCopy and WaitForPacket enabled for all tests

    NoIsolation.dat

    EtherCAT_Task + TX/RX IRQs on CPU1

    TX_IRQ_Isolation.dat

    EtherCAT_Task + RX IRQ on CPU1, TX IRQ on CPU0

    TX_RX_IRQ_Isolation.dat

    EtherCAT_Task on CPU1, TX/RX IRQs on CPU0

    ksoftirq execution time (µs)

    Average:  134.9

    Max: 441.0

    Average:  57.8

    Max: 311.0

    Average:  38.7

    Max: 113.0

    TX IRQ execution time (µs)

    Average:  25.6

    Max: 94.0

    Average:  39.2

    Max: 60.0

    Average:  41.7

    Max: 156.0

    RX IRQ execution time (µs)

    Average:  17.8

    Max: 64.0

    Average:  76.0

    Max: 90.0

    Average:  82.6

    Max: 186.0

    EtherCAT_Task execution time (µs)

    Average:  720.2

    Max: 1220.0

    Average:  581.7

    Max: 744.0

    Average:  508.4

    Max: 836.0

    Notes

    For EtherCAT_Task execution time, max execution time of 1220.0 µs was observed at beginning of trace capture file.  Unsure of whether this is an accurate "maximum" time since the rest of the trace sits under ~950 µs

    The goal of moving TX IRQ to CPU0 was to allow the RX IRQ to run concurrently to have the WaitForPacket be able to respond quicker.

    Although this did improve most execution performances, it had limited overall performance due to a ~100µs sleep between the RX IRQ finishing and EtherCAT_Task starting again to finish execution. Note that this sleep is also seen when TX/RX were both on CPU1 in NoIsolation.dat, but it had less of an effect due to the extended ksoftirq execution times.  

    Large ksoftirqd execution times can be seen due to the irq being preempted by EtherCAT_Task. 

    Moving both TX and RX IRQs off of CPU1 and onto a separate core from EtherCAT_Task shows the most stable performance when it comes to ksoftirq and EtherCAT_Task.

    The performance data may look comparable to TX_IRQ_Isolation since RX and TX IRQs are on the same core so WaitForPacket is being delayed by TX IRQ execution. This configuration doesn't have the sleep that we were seeing in TX_IRQ_Isolation and NoIsolation.

    The maximum ksoftirq execution time measured (113 µs) was due to an interrupt from ktimers. This was a one time occurrence in the trace unrelated to the network traffic, so expected maximum ksoftirq execution time can be expected to be closer to ~70 µs

    Like Daolin said above, with WaitForPacket enabled EtherCAT_Task is practically guaranteed to be interrupted by the IRQs which we believe is due to how WaitForPacket is designed to work. The best we saw to reduce the time interrupted was with the CPU isolation configurations above, but even then we are limited by only having two A53 cores on the AM64x. There is simply not enough processing power available to run the CODESYS child tasks and EtherCAT_Task without some sort of interruptions or delayed. As Daolin said above it may be beneficial to look into an R5 compatible EtherCAT stack so that you can utilize the R5 cores on the AM64x.

    -Rohit 

  • Hi Daolin,

    never mind, as we're also a bit behind our schedule to (re-)test with CPSW :-/ First tests both with PRU-ETH and CPSW doesn't seem that bad, we'll expect to have detailed measurements by this week.

    We already suspected that the inter-processor communication between A53 and R5 could be the next/worse bottleneck when moving the IRQ processing to the R5's, but anyway: Good to have this confirmed, so we can definitely rule that out.

    As to your question, if we already thought about an EtherCAT stack running on R5 cores: Yes, we definitely did. But due to the fact that the user application part of the EtherCAT processing today is user-programmable in CODESYS and they aren't able to generate code for R5, we'd always would need some inter-processor communication between A53 and R5 which is performant enough in terms of latency to satisfy the EtherCAT cycle time requirements. Anyway, if there is anything we might have overseen there, we'd be happy to hear about.

    Thank you very much for the continued, detailed support on this!

    -Florian

  • Hi Florian, 

    Apologies for the delayed response!

    never mind, as we're also a bit behind our schedule to (re-)test with CPSW :-/ First tests both with PRU-ETH and CPSW doesn't seem that bad, we'll expect to have detailed measurements by this week.

    Just wanted to follow-up with you on this. Your last response indicated that there was some detailed measurements to be collected on your end. Is there any additional items you need our support on?

    Thanks,

    Daolin

  • Hi Daolin,

    we repeated our tests as discussed with XDP zero-copy on CPSW with the other interface on PRU-ETH with core isolation, pinning and interrupt prioritization and WaitForPacket=TRUE.

    In the end, we see comparable results as you/Rohit showed: Due to only having the two cores, EtherCAT_Task keeps being interrupted as needed by WaitForPacket=TRUE.

    As for now, we cannot change the chosen processor type by replacing it with a higher core-count type. Though, further testing with AM62xP is planned with respect to future development for EtherCAT applications.

    Latest test we're about to do still on AM64x will be to activate busy-polling on XDP socket within CODESYS Runtime with the idea to then have interrupt-less operation of the data transfer. This is still on-going.

    Best regards,

    -Florian 

  • Hi Florian,

    Thanks for getting back to me on your latest tests. 

    As for now, we cannot change the chosen processor type by replacing it with a higher core-count type. Though, further testing with AM62xP is planned with respect to future development for EtherCAT applications.

    This is unfortunate but good that you were able to see comparable results to us. Yes, AM62xP is a more appropriate processor to not only give more flexibility for tuning parameters but we've also observed the 32-bit DDR provides close to 2x cycle time improvement.

    Latest test we're about to do still on AM64x will be to activate busy-polling on XDP socket within CODESYS Runtime with the idea to then have interrupt-less operation of the data transfer. This is still on-going.

    Let us know if you need more assistance with this later on. I'll keep this thread open in case there are further questions but please note that if there is no activity after two weeks the thread will automatically close. At that point, it is best to create a new thread.

    Thanks,

    Daolin