This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem using multiple USB client devices on dm6446

Hi,

I'm having problem using multiple USB client devices on our dm6446 base system. We have a hub attached to the usb port of the dm6446 and a cellular modem and external gps module attached to the HUB. Both devices are recognize by the system but everytime we try to use one device (gps via usb2serial), we are not able to access the cellular module port.

Is this a limitation on the HW of the dm6446 or this is a USB driver issue and is there a patch available we can use. Below is our configuration.

   DM6446 running Linux 2.6.18_pro500 (MontaVista0

   LSP_2_00_00_06

  MVL5

Thanks for the help!

-clint