This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP3503 UART Boot up issues



 

When using the OMAP3503DCBB

We first boot an OMAP in UART boot mode, the OMAP transmits a few ascii characters to tell the loader software on the terminal end when it is ready. We usually see something like a 40W or a 40T depending on the version of the processor.

I have a few on my desk that are putting out the hex codes 04 01 FD which do not translate to any meaningful ascii character.

On the boards that work, the characters 40W are the first printable ascii characters transmitted, but they are not the first data transmitted. Both designs start with the same three characters 04 01 05. The boards that do not work, hang after the 05, the boards that works continues to transmit more data, some of which is the 40W characters. Do you know what would cause the OMAP to stop transmitting any serial data after only three characters? Power is still there, clock is still present.

I can boot from SD Card on both boards.

Any ideas on the cause for this?

Charles