1. Ti DM8148 Android SDK has been released? Or not yet?
2. DM8148 through pin-mux registers 0x48140A58 ~ 0x48140AB8 can change video-in pins into camera input (16bit). The question is that can A8 unit inside DM8148 directly access these pins?
3. If yes then is there example code?
4. If no then only HDVICP2 unit can access the camera pins?
5. If yes then is there example code?
6. If no then how to access the camera pins to get image data?
Does the TMS320DM814x DMSoC Imaging Subsystem (ISS),User's Guide require and NDA? If so what is the procedure to download once I have an NDA in place