Part Number: AM5728
Hi,
we are using four AM5728 based modules along with KSZ9031 Phy for etherent. in the backplane, a switch(KSZ9896) is being used. when try to connect all four modules to switch at 100mbps, link toggling is observed continousely. as a fall back measure, when i try to reduce the link speed with 10mpbs , link is stable.
alternatively, i tried only two modules to switch at 100mbps and the link is stable. but if i restart any module(through init 6 command) and hold at u-boot stage, again i observed link toggling.
requeseted to guide me with the debugging as why link is stable in normal operation and toggling when one module held at u-boot.
regards,
Leeladhar