Other Parts Discussed in Thread: DM3730
Hello,
I have cross compiled mtd-utils for DM3730
I followed the instruction available at http://processors.wiki.ti.com/index.php/MTD_Utilities#MTD-Utils_Compilation and used arm-none-linux-gnueabi instead of arm-arago-linux-gnueabi
It builds successfully but after
make install DESTDIR=/home/user/mtd/install
the binaries in sbin folder is not working on the target machine.
For example i copied flash_erase to the target : adb push flash_erase /
Then i execute it with : adb shell ./flash_erase
It show the following error:
flash_erase: not found
I have also tried it after changing its permission but still gives the same error.
the properties for flash_erase are as show below:
flash_erase: ELF 32-bit LSB executable, ARM, version 1 (SYSV), dynamically linked (uses shared libs), not stripped
Please Help!
Thanks
Please Help.