This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCSTUDIO: the watch window

Part Number: CCSTUDIO
Other Parts Discussed in Thread: AM2612

Hi all,

Is it true that the variable order in the Expressions (Watch) window cannot be rearranged in the newer versions of CCS? Is it also impossible to add additional Expressions windows, or dock the window to the bottom or right side?
Furthermore, is it true that we cannot insert breakpoints on the fly while the processor is running?
Also, during debugging, how do I command multiple cores to run simultaneously? Currently, I have to manually click 'image.png' for each core one by one.
 
Regards,
Jenney